The energy transition needs flexibility: The CharIN Conference held at Phoenix Contact shows the path from charging to a connected energy system
As the stage for the CharIN Conference held from September 22 to September 25, 2026, the Phoenix Contact headquarters in Blomberg, Germany became the gathering place for an international network dedicated to the further development of charging infrastructure. The international event, which drew more than 350 participants, made it clear that the future of e-mobility extends far beyond the transportation sector and will continue to be developed as an integral part of a connected and sustainable energy system.
This is because e-mobility is increasingly evolving from a purely transportation-related subject into a central component of the energy transition. Against this backdrop, representatives from the energy sector, industry, research, and charging infrastructure gathered at the CharIN Conference hosted by Phoenix Contact to discuss how the next stage of e-mobility can be realized from both a technical and economic perspective. This was also the focus of the presentation by Ulrich Leidecker, COO of Phoenix Contact. “Building a scalable charging infrastructure will only succeed if vehicle manufacturers, charging infrastructure providers, technology companies, and energy companies work together to provide solutions”, he emphasized. Claas Bracklo, Chairman of CharIN e.V., pointed out that the charging ecosystem is becoming increasingly international and broad-based. “In addition to passenger cars, utility vehicles, buses, maritime applications, aviation, mining, and the energy sector are also taking part in the development of shared charging solutions”.
In addition to the conference itself, which featured expert presentations and discussions, participants had access to a test site where the charging compatibility of electric vehicles and electric trucks was put to the test in a practical setting. To verify the compatibility of their systems, technicians and engineers tested vehicles in the development stage at various EV charging stations. The aim was to test the interaction between different vehicles, EV charging stations, and systems.
The CharIN Conference also demonstrated that the technical prerequisites for intelligently networking mobility and energy are largely being satisfied. However, for these solutions to be widely adopted, we not only need technical advancements but also appropriate regulatory frameworks, expedited approval processes, and viable market models. Flexibility, interoperability, and the intelligent integration of vehicles, energy storage systems, and renewable energies are considered key factors for the success of the energy transition.