New holder for CCS type 2 charging connectors

2026-10-15
Holders for CCS type 2 charging connectors

Phoenix Contact is extending its e-mobility portfolio with a charging connector holder for CCS type 2 charging connectors. The robust holder enables the CCS charging connector to be seated securely on public and commercial DC charging stations.

A locking mechanism holds the inserted charging connector reliably in place. For removal, a simple press on the push button is all that is needed to unlock it. An optional microswitch in the charging connector holder also enables the EV charging station to monitor whether the charging connector has been reseated correctly. This feature supports the smooth operation of the charging infrastructure.

The charging connector holder protects the mating face and the contacts on the charging connector against environmental factors and mechanical damage. This helps reduce wear and maintenance requirements. The glass-fiber-reinforced, high-performance PA6 plastic ensures a long service life for the holder. When plugged in, the solution meets the IP55 degree of protection.

The holder is compatible with all standard-compliant CCS type 2 charging cables. In addition, it is suitable for customized mating face contours in accordance with IEC 62196-3:2026 and IEC PAS 63472:2023.

Press Contact
Eva von der Weppen
Eva von der Weppen | Corporate Communications