Connector temperature-rise test

Electrical tests for connectors and electronics housings High quality through optimum alignment of the current flow and voltage characteristics in test batch C

During electrical quality tests, the current and voltage characteristics of PCB terminal blocks, connectors, and electronic housings are examined. In our test laboratory, our engineers test the materials for their insulation and current carrying capacity properties, for example. They also measure the contact resistance prior to and after a test sequence.

As the third milestone prior to series release, test batch C consists of the following tests:

  • Cyclical overload test (heat-cycling test in accordance with UL 1059)

  • Cyclical aging test

  • Thermal reliability

  • Insulation resistance (UL 1703, UL27)

  • Current carrying capacity derating curve (IEC 60512-5-2)

  • Contact resistance measurement (IEC 60998-2-1)

  • High-voltage test

  • Impulse withstand voltage test (IEC 60664-1)

  • Air clearances and creepage distances

  • Resistance measurement

SUNCLIX connectors during the wet insulation resistance test

SUNCLIX connectors during the wet insulation resistance test

Wet insulation resistance test in accordance with UL 1703, UL 27

Connectors permanently in use outdoors must be able to withstand wind and weather for up to 25 years. The insulation materials used must reliably protect the users in the long term from dangerous body currents. The wet insulation resistance test offers a quantitative measure for the insulation performance of the test object. By performing the test in a conductive aqueous solution at rest, changes in the air clearances and creepage distances are identified, for example, through hairline cracks.

Series-connected male connectors in the Phoenix Contact test laboratory

Current carrying capacity test on male connectors at various temperatures

Current carrying capacity in accordance with IEC 60512‑5‑2

The current carrying capacity of a connector is limited by the thermal properties of the materials used for the contacts and connections as well as by the insulating parts of the housing. It is dependent on the self-heating and the ambient temperature at which the component is operated. The current carrying capacity derating curve reflects the ratio of the permissible current at the temperature present.

Impulse withstand voltage test in the Phoenix Contact laboratory

Impulse withstand voltage test in the laboratory

Impulse withstand voltage test in accordance with IEC 60664‑1

The impulse withstand voltage test provides the evidence of sufficiently large air clearances and creepage distances between two neighboring potentials. The magnitude of the test voltage is based on the rated surge voltage of the component. With three voltage surges (1.2/50 µs) per polarity, there must be no sparkovers. This test confirms that the components are safe to use in operation. The oscilloscope shows the time curve for a surge voltage pulse.

Connector voltage-drop test

Connector voltage-drop test

Volume resistance measurement in accordance with IEC 60998‑2‑1

A gas-tight connection ensures a continuously reliable electrical contact. Determining the electrical transfer resistance, typically before and after a test sequence, assesses the high quality of a connection.

Brochure
Tested quality – with safety
PCB terminal blocks and PCB connectors are among the basic elements in device manufacturing. They must not only be reliable but, within the scope of miniaturization, also increasingly smaller and more robust. Learn which tests and inspections Phoenix Contact device connection technology have to pass before series release.
Open and download PDF
A device developer examining a high-current feed-through terminal block