IRT managed switches

IRT managed switches

The FL SWITCH IRT range uses the ERTEC controller, and is therefore ideally suited for PROFINET applications. These switches fulfill all requirements for the optimum forwarding of PROFINET packets. With their integrated PROFINET device, FL SWITCH IRT devices can be fully configured and monitored by the controller.

Screenshot: Prioritized PROFINET data transmission

PROFINET prioritization

Prioritized PROFINET data transmission

Irrespective of the priority of the data packets, PROFINET packets are processed preferentially, which is done by searching the header file of the incoming packets for a PROFINET ID.

If a PROFINET ID is detected in the header, this data packet is processed with the highest priority. This provides the option of increasing the priority of certain applications, such as video streams, without impairing PROFINET communication.

This means that the system operator does not have to deal with prioritizing of PROFINET packets. This simplifies network planning, and it is possible to distinguish in detail between the priorities of all non-PROFINET telegrams.

Extremely short latencies are achieved when forwarding packets when transmitting in 100 Mbit operation – with the support of cut-through switching technology. This means that PROFINET packets quickly reach their destination, even via several switches.

Screenshot: IRT switch configuration

IRT switch configuration

Integration into engineering

You can fully configure the FL SWITCH IRT via the PROFINET controller – from initial startup including IP address assignment via DCP through to the port configuration.

During operation, the entire diagnostics for the IRT switches can be read out and monitored via the PROFINET device.

Fast device replacement and monitoring of the network topology is realized via the LLDP (Link Layer Discovery Protocol) defined in the PROFINET standard.

Screenshot: Diagnostics for fiber-optic cable paths

Diagnostics for fiber-optic cable paths

Diagnostics for fiber-optic cable paths

Via PROFINET, the FL SWITCH IRT can diagnose fiber optic paths and make the diagnostic data available to the controller.

This allows the quality of the fiber-optic cable path to be continuously monitored. To improve assessment of the fiber optic path, the IRT switches also make the path distances between two devices available to the maintenance engineer.

Screenshot: Switch-over in the event of an error

Switch-over in the event of an error

MRP – Fast and guaranteed switch-over time

Through their support of the Media Redundancy Protocol (MRP) ring redundancy mechanism, the FL SWITCH IRT devices safeguard the uninterrupted flow of data traffic in your network. As a part of the IEC 62439 standard, MRP guarantees maximum switch-over times of 200 ms in the event of an interruption.

You can also activate the MRP manager function in your IRT switch with the interchangeable FL MEM PLUG/MRM configuration memory. This function allows the switch to monitor the redundancy function for the entire MRP ring. In addition, you can save the device configuration to the external memory so you can replace a device in just a few seconds.

Overview of FL SWITCH IRT

The important data at a glance:

FL SWITCH IRT

Transmission speed 10/100 Mbps
Alarm contact Yes
Temperature range -25°C ... +60°C
Supply voltage 18.5 ... 30.2 V DC (redundant)
Filter functions
Quality of Service Yes
VLAN No
Multicast / IGMP snooping No
Redundancy
Rapid Spanning Tree (RSTP) No
MRP manager/client Yes (optional) / yes
Fast Ring Detection (FRD) No
Large Tree Support No
Management functions
Port configuration, statistics, and utilization Yes
Link Layer Discovery Protocol (LLDP) Yes
Address Conflict Detection (ACD) No
Automation protocols
PROFINET Conformance Class C
PROFINET device Yes
EtherNet/IP™, extended multicast filtering No
Approvals/certificates
Maritime approvals No
Ex approvals No
To the product list