Utilize field data easily with Industrial Ethernet
Artificial intelligence is being used ever more frequently in industrial applications. With the third generation of the Valueline product family, Phoenix Contact is providing industrial PCs that meet these demands.
Using the Intel Tiger Lake UP3 series, Valueline IPCs now include the 11th generation Intel Core i7/i5/i3 and Celeron processors for industrial use. In terms of robustness and reliability, only components that ensure smooth operation of the IPC at temperatures from -20°C to 50°C are selected. In terms of connectivity, even the basic version of the Valueline product family supports numerous current communication interfaces. If the existing interfaces are not sufficient, additional interfaces can be configured easily via the integrated I/O extension module. When configured as a panel PC, the latest touch drivers are integrated so that operation is possible even when wet or when wearing gloves. Displays ranging in size from 15.6 inches to 21.5 inches (1920 x 1080 pixels) in full HD provide enough space for visualizing both simple procedures and complex production processes.