New PCB connectors open up design freedom
The new SPC 4 PCB connector series from Phoenix Contact saves space and production costs with its customer-oriented design.
With a pitch of just 6.35 mm, the PCB connectors of the SPC 4 series now take up even less space on the device. In combination with the enhanced shield contacting innovation, completely new design freedoms are opened up in the design-in process. The THR headers on the SPC 4 series enable automated assembly, reducing production costs. In addition, this sophisticated series also has reflow soldering capability. The proven Push-in connection makes installation easy, and large conductors up to 4 mm² can be used. With extended touch protection on the header and plug, the connector also provides added value in terms of safety.