Vote now: Mini Analog Pro highly compact Ex i signal conditioners with SIL 3 are a finalist for the GIT Security Award
The Ex i signal conditioners and measuring transducers of the proven 6.2 mm Mini Analog Pro product family have been nominated in category B: “Occupational Safety and Health & Explosion Protection” for the final round of voting for the GIT Security Award.
Whether in the classic process industry or modern power-to-X systems, explosion protection and the safety of people, systems, and the environment are very important. At the same time, products need to deliver the same or superior functionality while becoming smaller and more efficient. The Mini Analog Pro highly compact Ex i signal conditioners and measuring transducers with SIL 3 set a milestone in miniaturization: They offer explosion protection and functional safety in a compact design, providing space savings of up to 50 percent in the control cabinet compared to conventional solutions. The operating concept, configuration and monitoring app, communication gateways, digital tagging, and digital nameplate are particularly user-friendly and future-proof.
A neutral jury preselected the nominees for the final round of voting for the international award that is presented by the trade journal “GIT Security” published by Wiley. The jury is made up of experts from industry associations such as BHE, TÜV, VDMA, and ZVEI, as well as system integrators and users. The award recognizes the innovativeness, benefits, and unique features of products in various categories. The top three winners in each category will be determined by the votes cast by readers on the international, cross-industry platform PRO-4-PRO.com, Products for Professionals.