Housing kits for the comprehensive protection and electrical connection of different PCBs
2023-03-27
Electronics housings provide safety and protection for the electronics. Housing kits from Phoenix Contact make it easier to select the entire housing for rapid prototyping.
Both for mechanical mounting on a DIN rail in accordance with DIN EN 60715 and outside the control cabinet, the tailored housing system provides a solid basis, plus integrable components for the interfaces. To accommodate an electronic circuit board including the corresponding connection technology, the kits contain all the components needed to assemble a complete housing that is ready to use straight away. In industrial electronics, this enables the fast and cost-effective implementation of individual devices and test setups, right up to small series.
Press Contact
Eva von der Weppen
|
Corporate Communications
eweppen@phoenixcontact.com