Battery holder for OCS and POS housings

2026-01-21
OCS Bat Hold battery holder set installed in an OCS housing

The new OCS Bat Hold battery holder from Phoenix Contact is specially designed for the OCS and POS series electronics housings.

It is used to securely fasten batteries in the 72 to 720 kWh range. Made of galvanized steel, the holder enables the simple installation of self-sufficient systems even under extreme ambient conditions. The space-saving solution leaves enough room for the installation of additional electronics. The holder consists of a battery mounting set and a mounting panel with base. Mounting the OCS Bat Hold is simple, requiring just one tool (AF 13).

Press Contact
Eva von der Weppen
Eva von der Weppen | Corporate Communications