Automated wiring for all types of conductors
In addition to the XTV terminal blocks with lateral conductor routing, the first terminal blocks with frontal Push-X connection are now available from Phoenix Contact. The XT portfolio consists of feed-through and multi-conductor terminal blocks as well as function versions for using disconnect knives, plug-in fuses, and components.
As one of the fastest connection technologies on the market, the new Push-X technology from Phoenix Contact increases the efficiency of control cabinet wiring. All conductor types and cross-sections can now be connected even faster, either manually or automatically. Direct wiring is carried out tool-free and without significant effort due to a pretensioned contact spring. By lightly tapping the release surface inside the clamping chamber, the contact spring is released and the conductor is contacted safely and permanently. As with Push-in technology, the connected conductors are released by pressing the orange push button. At the same time, the contact spring is pretensioned for the next wiring process.
All Push-X terminal blocks are fully compatible with the standardized Clipline complete terminal block system.