Germany builds blueprint for the All Electric Society
Project goal
Construction of a smart commercial property using modern technology for sector coupling as well as sustainable solutions.
Milestones
- Tangible example of sector coupling
- Cooling and heating network with heat pumps and ice storage tank
- Industrial DC power grid
- Variable room concepts
Investment amount
Battery storage systems
in the industrial DC power grid
With the All Electric Society Factory at its Blomberg headquarters, Phoenix Contact demonstrates the bidirectional coupling of all energy flows. This concept creates electrical, thermal, and communication connections between all energy-generating and energy-consuming components. The investment thus serves as a blueprint and tangible proof of a realistic All Electric Society – a world in which electricity generated without carbon emissions is the primary form of energy.
Buildings offer much more than just a roof over your head
They show how it’s done. And provide inspiration as to how the energy transition can be achieved with intelligent technology and integrated solutions. To this end, the All Electric Society Factory uses, for example, an ice storage tank for its heating and cooling needs, plus a photovoltaic system with 2.5 MWp and pioneering storage solutions. Here, Phoenix Contact relies on battery storage systems and hydrogen. Another feature that is incorporated into the blueprint for sustainable buildings is the installation of a DC power grid in conjunction with bidirectional charging technology. Here, e-cars also become temporary energy storage systems and supply the building. This is sustainable and smart at the same time. The ambitious project is valued at around €35 million and will serve as a blueprint for sector coupling when it is put into operation in 2023 during our anniversary year.
The All Electric Society Factory combines construction innovations in terms of energy efficiency and the reuse of building materials with forward-thinking industrial applications ranging from the generation to the use of renewable energies.
Forms of energy flow together here
Specifically, the company is building a thermal network at the local level – using heat pumps and a 1,500 m³ ice storage tank. The aim here is to integrate and utilize all waste heat from all processes. Electrically, the first stage will involve the use of battery storage systems, two photovoltaic systems, and a partial DC power grid. Connected to this is charging infrastructure for e-mobility. The installation of a DC power grid for industrial use is a deliberate strategic decision, as this will play a crucial role in driving the energy revolution forward – e.g., due to the improved integration capability of renewable energy sources, battery storage systems, and e-mobility, which are all based on direct current. In addition, power dissipation can be reduced effectively – for example, by using energy from regenerative braking in electric vehicles. The plan is to expand this blueprint for the All Electric Society to include industrial solutions involving hydrogen and power-to-X.