Sunclix crimp contacts for conductor cross-sections from 6 to 10 mm²

2026-06-17
Sunclix crimp contacts

With the new Sunclix crimp contacts for conductor cross-sections from 6 to 10 mm², Phoenix Contact is expanding its portfolio for powerful DC connections.

The contacts enable a current carrying capacity of up to 50 A. They are suitable for applications involving increasing direct currents, such as in device connection, field wiring, powerful photovoltaic panels, or long cable paths with minimized losses.

The contacts are available both in rolls and in polybags in various pack sizes. They are compatible with the Crimpfox SR 6 crimping tool, so existing crimping positions can continue to be used. Suitable crimping dies are available for automated production processes.

Press Contact
Eva von der Weppen
Eva von der Weppen | Corporate Communications & Brand Management