Subscription license for the Energy Management Service. Requires the Energy Management Service Pro license. Energy Management Service Custom setup requires the Custom license and vice versa. Operation and maintenance of a customized solution.
Energy, Monitoring, Management, Analytics with the EMMA Service
The EMMA Service in Proficloud.io, Phoenix Contact’s IoT platform, provides companies with user-friendly access to data that is crucial for energy management. This is aided by the specially designed dashboards of the Smart Service, all of which can be arranged with just a few clicks of the mouse. As a result, you can make decisions faster and more accurately, and workflows can be streamlined through remote monitoring.
Use the entire range of Energy Management Service functions. Unlimited data storage and availability. 100 metrics included. Unlimited number of users. Annual subscription. Unlimited use of functions.
The Energy Management Service scales with your company. Requires the Energy Management Service Pro license. Additional 100 metrics for use. Uncompressed data. Minute-by-minute resolution.
The Energy Management Service scales with your company. Requires the Energy Management Service Pro license. Additional 50 metrics for use. Uncompressed data. Minute-by-minute resolution.
Design draft for a customized Energy Management Service. Requires the Energy Management Service Pro license. Energy Management Service Custom setup requires the Custom license and vice versa. The company logo, color scheme, and URL can be customized.
The Energy Management Service scales with your company. Requires the Energy Management Service Pro license. Additional 200 metrics for use. Uncompressed data. Minute-by-minute resolution.
Learn about the Energy Management Service for your proof of concept (PoC). Unlimited number of users. Test period of 1 year.
Advantages of the EMMA Smart Service
-
High user-friendliness with a systemic overall concept and intuitive menu navigation
-
Targeted overview with intuitive visualization options
-
Optimized energy management, especially with regard to the international standard ISO 50001
-
Optimized workflows with location- and time-independent monitoring of energy and performance data
-
Automated data transmission to Proficloud.io when using the IIoT-capable EMpro energy measuring devices
EMMA Service functions
User-friendly dashboards and widgets:
With only a few clicks, users can draw initial conclusions about the processes and energy consumption. Use the various visualization options such as energy cycle diagrams, energy bar diagrams, streamline diagrams, heat maps, and Pareto diagrams.
Energy bar chart - load over load:
You can use this widget to compare the energy data of several loads next to each other over the same period of time. The data is displayed in a bar chart.
Energy bar chart – period over period:
With this widget, you can overlay energy data from several time periods for the same load in a widget. The data is displayed in a bar chart.
Energy pie chart – load over load:
This widget can be used to compare the energy data of several loads over the same period of time. The data is displayed with its absolute values and its relative share of the total consumption of the various loads on a pie chart.
Energy pie chart – period over period:
This widget can be used to compare energy data from several time periods for the same load. The data is displayed with its absolute values and their relative share of the total amount of the different consumption periods of a consumer on a pie chart.
Energy Pareto chart – organized by loads:
This widget shows the energy data of multiple loads over a selected period of time. The information is displayed in a combination of bar charts and line charts. A bar represents the total value for the selected period of time per load. The bars are sorted from the highest (left) to the lowest (right) consumption. The widget also contains the accumulated percentage value as a line chart.
Additional functions
- Power line chart - load over load
- Power line chart – period over period
- Heat map
- KPI/ENPI - Key performance indicators or energy performance indicators
- Use external data sources for your analysis
- Create simple reports with ENPIS based on your dashboards