Resetting the Device to Default Setting (without display)



 

Resetting the device to default settings (without display)

EMpro has various options for resetting the device to the default setting.

A reset to the default settings has the following effects:

  • All configuration parameters are reset to the delivery state
  • PIN and WBM password are reset to the delivery state
  • Device identifiers are reset to the delivery state
  • All resettable counters are reset
    • Resettable total energy meter
    • Tariff meter
    • Pulse counter
    • Resettable operating hours meter
  • Min/Max & Avg values are reset
  • The selection of the currently used tariff meter is discarded and no tariff is selected
  • All data logging records are deleted
  • The device restarts and is in the configuration wizard

Reset to default settings without PIN

Pressing the reset button for at least 5 seconds resets the device to the default settings. This reset option is only enabled for a period of one minute after restarting the device. No admin rights are required. After the button has been pressed for 5 seconds, the status LED starts to flash quickly. Pressing the button again while the LED is flashing first initiates the reset. If the reset mode is activated for 7 seconds and no action is taken by the user, it is exited again.

 


EMpro online documentation
Published/reviewed: 2025-07-15, en revision 003Version history