Data Types and Registers


What you will find in this section:

  1. Data types and registers
  2. Related topics

 

Data types and registers

 

The Modbus specifications does not include requirements on how various data types are to be displayed on the respective register.

 

Data encoding format used by EMpro is little-endian byte swap. The meaning for the arrangement of the transferred bytes (numeration in red) can be seen in the following figure (value to transfer as hexadecimal number).


 

Example of register allocations for different data types

8-bit integer types:
Example: Value = 1 (0x01)

 

Register address

Register contents (hex)

n

0x0001

 

16-bit integer types:

Example: Value = 4660 (0x1234)

 

Register address

Register contents (hex)

n

0x1234

 

32-bit integer types:

Example: Value = 305419896 (0x12345678)

 

Register address

Register contents (hex)

n

0x5678

n +1

0x1234

 

32-bit IEE 754 floating point:

Example: Value = 123.456 (0x42F6E979)

 

Register address

Register contents (hex)

n

0xE979

n +1

0x42F6

 

ASCII strings:

Example: Value = EEM-MA (0x45, 0x45, 0x4D, 0x2D, 0x4D, 0x41, 0x33, 0x37, 0x30 -> ASCII coded)

 

Register address

Register contents (hex)

n

0x4545

n +1

0x2D4D

n +2

0x414D

n +3

0x3733

n +4

0x0030

 

 


EMpro online documentation
Published/reviewed: 2025-07-15, en revision 003, Version history