Integrating Modules and Submodules


What you will find in this section:

  1. Integrating modules and submodules
  2. Related topics

 

Integrating modules and submodules

 

  1. In the structure tree, switch to the “Device configuration” view.
  2. In the hardware catalog, mark the desired module.
  3. Drag and drop it to the device overview.

 

Adding a module to the device overview
Adding a module to the device overview

 

Subsequently, the associated submodules appear in the catalog. 

 

Submodules in the hardware catalog
Submodules in the hardware catalog

 

  1. Select the desired submodules.
  2. Add the submodules under the respective main module using drag-and-drop.

 

Inserting submodules
Inserting submodules

 

The device overview shows the available modules and submodules.

 

Available modules and submodules
Available modules and submodules

 

  1. Select a configured submodule in the device overview.


If you are a Siemens user, refer to the register table for the respective energy measuring device for descriptions of the individual process data, which can be downloaded at phoenixcontact.net/products .

 

Selecting a submodule in the device overview
Selecting a submodule in the device overview

 

 


EMpro online documentation
Published/reviewed: 2026-07-10, en revision 004, Version history