Tariff Selection
|
Navigation on the display |
“Tar, Tariff meter 1...4“ |
The device offers various options for selecting between up to four tariffs. The following procedures are possible:
- Using the digital input: 2 tariffs can be used
- Using manual switching via a communication interface: 4 tariffs can be used
- Using a time schedule: 4 tariffs can be used