Data Logging

 

 

Menu: “Logging”
Menu: “Logging”

 

Status

The “Status” area shows an overview of the current logging data.

 

“Menu: Logging, Settings”
“Menu: Logging, Settings”

 

Log 1...8

Here, you can configure up to eight different logging parameters.

Data source

Select the desired electrical parameter for the logging from the drop-down menu.

Interval

Enter the interval time in minutes. The shortest duration that can be set is 1 minute.

The maximum logging duration depends on the configured interval. For an interval of 15 minutes, the logging capacity is approx. 90 days. If you shorten the interval, the logging capacity is also reduced (e.g., 10 minute interval/60 days logging capacity).

Circular buffer 

Activate the circular buffer if you want to use the FIFO principle (first-in/first-out) for the data logging.

Deactivate the circular buffer if you want to define a fixed starting point.

The logging automatically stops once the memory is full.

 

Menu: “Logging, Saved data”
Menu: “Logging, Saved data”

 

You can view all configured logging data as a chart in the web server.

To do so, select the desired logging data from the drop-down menu.

With your mouse, you can zoom in on the saved data.

By means of the selection box to the right next to the chart, you can also export the logging data as CSV, XLS or PDF file.

 


EMpro online documentation
Published/reviewed: 2025-07-15, en revision 003Version history