Description of the Register Table


What you will find in this section:

  1. Description of the register table
  2. Related topics

 

Description of the register table

 

Register table
Register table

 

Content of the line (CH)

The first line of the register table contains information about the content of the respective line or column.

 

H1 … Hn: Heading

An “H” with a number indicates a heading. The number behind it indicates the hierarchical level.

To keep the register entries structured and readable, they are divided by headings.

 

R: Register

The “R” stands for Register and designates the lines that each describe a register.

Only lines that also contain registers are relevant for automatic processing of the register table.

 

U: Unused

The “U” describes unused entries. These can be, e.g., address ranges that do not have a function (yet) and are reserved.

 

E: End

The “E” describes the end of the table.

 

Dec: Decimal address

The second column of the register table contains register addresses in decimal form.

 

Hex: Hexadecimal address

The third column of the register table contains register addresses in hexadecimal form.

 

Count

The “Count” column displays the number of registers required for the function described in this line. The required number is directly dependent on the data type.

 

Short designation

The “Short designation” column contains the abbreviated designations of the registers. The short designations are unique, so that all other data can be referenced using the short designations.

 

Unit

The unit for the process values is given in the “Unit” column. For example, the unit for the voltages is volt [V].

 

Divider

The “Divider” column states the divider by which the value is to be divided to get the correct value. This is necessary, e.g., if the data type is an integer value, but a decimal fraction has to be entered. 

Example:

If the harmonics are specified as percentage with signed integer, but have to be output with a precision of a tenth of a percent. In this case, for example, 15.2% is used as 152 with divider 10.

 

R/W: Read/write access

This column specifies which access is permitted for the respective register.

 

R: Read only

These registers can only be read. Attempting write access to these registers causes an error.

 

R/W: Read and write

It is possible to both read and write to these registers.

 

W: Write only

These registers can only be written. Attempting read access to these registers causes an error.

 

W/R0: Write only and read 0

These registers can only be written. Read access to these registers results in a zero as response.

 

Datatype

This column contains the data type to be used for decoding the contents of each respective register.

 

ASCII


Each register (16 Bit) contains two ASCII characters. When the number is entered, the number of individual registers contained in the character string is determined.

Example:

Dez:1234567

Hex: 0X31, 0X32, 0X33, 0X34, 0X35, 0X36, 0X37

Zero-terminated:     “12345670”

Hex: 0X31, 0X32, 0X33, 0X34, 0X35, 0X36, 0X37, 0X00

Number of registers = 4: Hex: 0X3231, 0X3433, 0X3534, 0X0037

 

Bit mask

Each bit (bit 15-bit 0) of the register (16 bit) is evaluated individually.

Example: “Resetting the tariff meter”

Bit 0: Reset tariff 1

Bit 1: Reset tariff 2

Bit 2: Reset tariff 3

Bit 3: Reset tariff 4

An individual tariff meter, or any combination of meters from all tariff meters can be reset.

 

Bool

This data type makes a logical statement.

0: false

1: true

 

Fl32

IEEE-754-single number 1.8.23 (32 bits, two 16-bit registers):

1 sign bit: positive and negative

8 exponent bits: ≈ value range of 38 decimal places

23 mantissa bits: ≈ precision of 6 decimal places

Decimal value range: ±1.175·10-38 to 3.40282·1038

 

Register in float

32-bit value from the registers: 0X41340000 = 01000001 00110100 00000000 00000000b

Bit31 = 0: SB, sign bit. This number is positive.

Bit30 - Bit23: E, exponent. In this case: 130.

Bit22 - Bit0: M, mantissa. Here it is 3,407,872.

Z = 11.25

Float in register

Floating-point number X = 11.25

SB, sign bit. This number is positive => Bit31 = 0 / 0X00 / 0b

In this case 130 => Bit30 - Bit23 = 130 / 0X82 / 10000010b

mantissa. Here it is 3,407,872 => Bit22 - Bit0 = 3407872 / 0x340000 / 0110100 00000000 00000000b

32-bit value for the register: 0X41340000 = 01000001 00110100 00000000 00000000b

SInt16

Signed integer:

2 byte, 16 bit

Value range:     -215 … 215-1

-32,768 … 32,767

UInt16

Unsigned integer:

2 byte, 16 bit

Value range:     0 … 216-1

0 … 65,535

UInt32

Unsigned integer:

4 byte, 32 bit

Value range:     0 … 232-1

0 … 4294967295

SInt32

Signed integer:

4 byte, 32 bit

Value range:     -231 … 231-1

-2,147,483,648 … 2,147,483,647

UInt8

Only the low byte of the register is evaluated.

1 byte, 8 bit

Value range:     0 … 28-1 = 0 … 255

UInt[]

Array of UInt8 values. Their order follows that of the ASCII registers.

These data types are used, e.g., for the MAC addresses. 

Three registers are required for the six bytes. 

E.g., 00:A00:45:66:4F:41

Name

Here, the name of the respective register is entered. It may be longer than the short designation, so that it is readable and expresses the function of the register.

Description


In this column, the function of the register is described in detail.

 

 


EMpro online documentation
Published/reviewed: 2025-07-15, en revision 003, Version history