Inserting Cable Ducts
Cable ducts are inserted from the Cable ducts category in the Insertion Center via drag & drop. They can be placed on mounting plates or used with wall boxes.
Edit cable duct
You can edit a cable duct as follows:
| To... | Do the following... |
| Adjust length of cable duct |
- Place the mouse cursor on the end of the cable duct to display the double arrow and drag the mouse leftwards or rightwards while keeping the left mouse button pressed.Or
- In the radial menu of the cable duct, select the Change cable duct length command and enter the length in the appearing dialog.
The maximum length is limited by the length of the mounting rail. |
| Rotate cable duct by 90° | In the radial menu of the cable duct, select the Rotate by 90° command.The cable duct is rotated clockwise or counterclockwise (depends on the current rotation) around the object's center.
Note
If there is not enough space on the mounting plate to place the rotated cable duct, the cable duct is attached to the mouse cursor until you drop it on a valid position. |
|