NACS charging
Parameter dependancies If PAR_InletType is set to NACS the following parameter needs to be set to specific values: PAR_TempConfiguration needs to be set to NACS_XXX
PAR_HVSWSink needs to be set to VCU_CAN
NACS HVSW support
The CHARX EVC-100 supports Function till ASIL-B Switch control in case of NACS it is rated with ASIL-D due to commen usage of path for AC and DC, so the CHARX EVC-100 can't take over this function