Error descriptions

Enter the error code you are looking for in the search field:

1: DET

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 ERROR_MEMORY_FULL Error memory is full, no further error entries can be stored -
2 WRITE_ERROR_NEW Error while writing a new error entry to NVM ID of the module whose error entry can't be created
3 WRITE_ERROR_MODIFY Error while modifying an error entry in the NVM ID of the module whose error entry can't be modified
4 WRITE_ERROR_DELETE Error while deleting an error entry from NVM ID of the module whose error entry can't be deleted

2: BSW

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened

3: CAN_CFG

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened

4: FLASH_IF

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 ERASING Error while erasing memory block Status which leads to this error
2 ERASE_VERIFY Error while verify erased memory block Status which leads to this error
3 PROGRAMMING Error while programming memory chunk Start address of the memory chunk that causes the error
4 PROGRAM_VERIFY Error while verify programmed memory chunk 0xFFFFFFFF = At programming end: To less or to much bytes programmed Else = Address where verify failed

5: PAR_IF_COMMON

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 WRITE_EEPROM Write to Eeprom/NonVolatileMemory failed

0 = StayInBootloader flag

1 = Bootloader parameter

2 VERIFY_EEPROM Write to Eeprom/NonVolatileMemory failed

0 = StayInBootloader flag

1 = Bootloader parameter

6: PAR_IF_BL

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 STAY_IN_BL "Stay in bootloader" flag can't be set -

7: BOOT

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 START_PROGRAM Problem starting application -
2 VERSION_TO_OLD Firmware version is to old Old / stored firmware version

8: CMS_GATEWAY

Reason ID Reason Description Additional Data

0

ASSERT

Used by the assert function

Line number in which the assert happened

1

TIMEOUT_NONE_EMPTY_RB

Forward timeout happened while still messages in buffer

Number of entries in buffer

2

SENDING_ERROR

Error while sending a CAN message

Error reason (status_t)

3

RB_FULL

Ring buffer is full

Ring buffer instance (0 =VCU, 1 = CMS)

4

UNKNOWN_CAN_ID

Gateway detected an unknown CAN ID

The unknown CAN ID

9: UDS

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 NOT_SUPPORTED_RESET_REQUESTED Used by the assert function Reset type which leads to this error

10: ISO_TP_IF

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 RECEPTION_ERROR Error while receiving an IsoTP message Reason for this error

11: ISO_TP

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened

12: VERSION

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened

13: OS_TASKS

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 CLOCK Error while initialize system clock

1 = INITIALITATION_ERROR

2 = UPDATE_ERROR

2 SBC_ERROR Read out of SBC errors is not equals zero Error count
3 WDOG_TRG_IN_INIT_LATE Watchdog was not triggered in time while initialization.

Byte 0-1: Time since last watchdog trigger

Byte 2-3: Number of calls of watchdog trigger

14: EEPROM_IF

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 INIT_PARTITIONING_FAILED Unable to partition FlexNVM for Eeprom emulation Status which leads to this error
2 INIT_ENABLE_EEE Unable to configure FlexRAM for Eeprom emulation Status which leads to this error
3 INIT_EEPROM_NOT_READY Unable to configure FlexRAM for Eeprom emulation Status which leads to this error
4 WRITE_FAILED Write to Eeprom failed Status code of the operation
5 VERIFY_DISABLE_EEE Disabling Eeprom emulation while verify failed Status code of the operation
6 VERIFY_ENABLE_EEE Enabling Eeprom emulation while verify failed Status code of the operation
7 VERIFY_COMPARE Data compare failed. Source and destination differ Address of the destination
8 QUERY_EEE_STATUS Querying Eeprom emulation status failed Status code of the operation
9 MAINTENANCE_FAILED Maintenance of quick write data failed Status code of the operation
10 QUICK_WRITE_DATA_LOSS Data loss due to brown out while quick write -
11 NORMAL_WRITE_DATA_LOSS Data loss due to brown out while normal write -
12 UNKNOWN_EEE_STATUS Eeprom emulation status is unknown Unknown status value
13 QUICK_WRITE_MAINTENANCE_NECESSARY Quick Write maintenance required, although Quick Write is never used -
14 VERIFY_WAIT_TIMEOUT Waiting for Eeprom emulation ready timed out while verify failed -
15 JTAG_UNLOCK_FAILED Unlocking the JTAG failed -
16 REINIT_EEPROM_NOT_READY Unable to re-enable Eeprom emulation -
17 REINIT_ENABLE_EEE Unable to configure FlexRAM to re-enable Eeprom emulation Status which leads to this error

15: PLATFORM_IF_BL

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 RESTART_MCU_FAILED Restart of microcontroller via SBC auto wake-up failed SPI response code (status_t)
2 HW_CODE_INVALID Not supported hardware Measured hardware code resistor value
3 ADC_CONVERSION_TIMEOUT HWCode_VFB ADC conversion timeout -

16: SECURITY_IF

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 CSEC_UNINITIALIZED The CSEc is not correctly initialized

byte 3 & 2: status_t of the function call that failed

byte 1 & 0: The line number in which the error occurred

2 KEY_SLOT_WRITE_FAILED Writing one of the CSEc's key slots failed

byte 3 & 2: status_t of the function call that failed

byte 1 & 0: The line number in which the error occurred

3 RANDOM_FAILED Generating a random value failed

byte 3 & 2: status_t of the function call that failed

byte 1 & 0: The line number in which the error occurred

4 AES_FAILED A AES crypto operation failed

byte 3 & 2: status_t of the function call that failed

byte 1 & 0: The line number in which the error occurred

5 NO_VALID_RS256_KEY_FOUND No RS256 key for signature validation has been found or the key is invalid

byte 3 & 2: status_t of the function call that failed

byte 1 & 0: The line number in which the error occurred

17: EEPROM_MANU_IF

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened

18: SBC

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 INIT_PARTITIONING_FAILED Unable to partition FlexNVM for Eeprom emulation Status which leads to this error
2 INIT_ENABLE_EEE Unable to configure FlexRAM for Eeprom emulation Status which leads to this error
3 INIT_EEPROM_NOT_READY Unable to configure FlexRAM for Eeprom emulation Status which leads to this error
4 WRITE_FAILED Write to Eeprom failed Status code of the operation
5 VERIFY_DISABLE_EEE Disabling Eeprom emulation while verify failed Status code of the operation
6 VERIFY_ENABLE_EEE Enabling Eeprom emulation while verify failed Status code of the operation
7 VERIFY_COMPARE Data compare failed. Source and destination differ Address of the destination
8 FW_TRIGGER_OS_REGULAR FW: Triggering of SBC in normal process failed SPI response code (status_t)
9 FW_TRIGGER_EEPROM FW: Triggering of SBC while EEPROM process failed SPI response code (status_t)
10 FW_RESET_MCU FW: Restart of microcontroller via SBC auto wake-up failed SPI response code (status_t)
11 FW_GET_FAULT_COUNTER FW: Read of SBC fault counter failed SPI response code (status_t)
12 FW_RELEASE_FS0B FW: Releasing of FS0B of SBC failed SPI response code (status_t)
13 FW_REQUEST_FS0B FW: Requesting of FS0B of SBC failed SPI response code (status_t)
14 FW_SET_LOW_POWER_MODE FW: Setting of low power mode of SBC failed SPI response code (status_t)
15 FW_SET_WAKE_UP_SRC FW: Setting of wake up sources of SBC failed

Byte 0 ... 1: SPI response code (status_t)

Byte 2 ... 3: Line number in which the error happened

40: INLET_CTRL

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 NOT_OPEN_IN_OPEN_STATE Lock feedback is not open in open state Lock state determined by the ADC feedback values
2 NOT_CLOSE_IN_CLOSE_STATE Lock feedback is not close in close state -
3 LOCKING_TIMEOUT Timeout error while closing -
4 RELEASING_TIMEOUT Timeout error while releasing 0 = Single feedback / single diag feedback 1 = Endstop diag feedback
5 LOCKFBK_SHORT_TO_GND Short to GND between fbk+ fbk-

Byte 0-1: ADC value of LockFbk_CFB

Byte 2-3: ADC value of LockFbk_VFB

6 LOCKFBK_SHORT_TO_BAT_OR_OL Short to BAT or open load between fbk+ fbk-

Byte 0-1: ADC value of LockFbk_CFB

Byte 2-3: ADC value of LockFbk_VFB

7 LOCKFBK_OUT_OF_RANGE Measured resistance is out of range of the configured parameters

Byte 0-1: ADC value of LockFbk_CFB

Byte 2-3: ADC value of LockFbk_VFB

8 LOCKFBK_PARAMETER_OVERLAP Configured parameters do overlap -
9 LOCKFBK_PARAMETER_MIN_GREATER_OR_EQUAL_MAX Configured parameter MIN >= MAX -
10 LOCKFBK_PARAMETER_NOT_DIAGNOSABLE Configured parameter < 500Ohm and therefore cannot be diagnosed -
11 SELFTEST Error detected in selftest

Byte 0-1: ADC value of LockFbk_CFB

Byte 2: 0: Parameter invalid 1: Parameter valid

12 STATE_MACHINE Error processing a state machine

0 = Default state activated

Else = Line in which the error happened

13 LOCKFBK_MALFUNCTION Lock feedback measurement is faulty.

Byte 0-1: ADC value of LockFbk_CFB

Byte 2-3: ADC value of LockFbk_VFB

41: LED_CTRL

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 INTENSITY_INVALID Led intensity is invalid intensity in 1 per mill

42: SWITCH_CTRL

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
2 STATE_MACHINE Error while process a state machine Line number in which the error happened
3 UNKWON_CONNECTION_TYPE Unknown connection type (Not directly nor via CAN) Value which leads to this error
4 SWITCH1_SHORT_TO_BAT_HS HV-Switch 1: Short to battery (probably on the high side) Byte 0-1: ADC value of HS_VFB Byte 2-3: ADC value of LS_VFB
5 SWITCH2_SHORT_TO_BAT_HS HV-Switch 2: Short to battery (probably on the high side) Byte 0-1: ADC value of HS_VFB Byte 2-3: ADC value of LS_VFB
6 SWITCH1_SHORT_TO_BAT_LS
7 SWITCH2_SHORT_TO_BAT_LS
8 SWITCH1_OPEN_LOAD
9 SWITCH2_OPEN_LOAD
10 SWITCH1_SHORT_TO_GND_HS
11 SWITCH2_SHORT_TO_GND_HS
12 SWITCH1_SHORT_TO_GND_LS
13 SWITCH2_SHORT_TO_GND_LS
14 SWITCH1_DIAG_DEFECT_HS
15 SWITCH2_DIAG_DEFECT_HS
16 SWITCH1_NO_POWER_SUPPLY
17 SWITCH2_NO_POWER_SUPPLY
18 SWITCH1_FS0B_NOT_RELEASED
19 SWITCH2_FS0B_NOT_RELEASED
20 SWITCH1_SBC_COM_ERROR
21 SWITCH2_SBC_COM_ERROR
22 SWITCH1_OVER_LOAD
23 SWITCH2_OVER_LOAD
24 SWITCH1_STATE_COMBINATION
25 SWITCH2_STATE_COMBINATION
26 SWITCH1_WELDED
27 SWITCH2_WELDED
28 SWITCH1_REPORTED
29 SWITCH2_REPORTED
30 SWITCH1_OPEN_LOAD_OR_SHORT_TO_BAT
31 SWITCH2_OPEN_LOAD_OR_SHORT_TO_BAT
32 SWITCH1_OPEN_LOAD_OR_SHORT_TO_GND
33 SWITCH2_OPEN_LOAD_OR_SHORT_TO_GND
34 SWITCH1_UNKNOWN_ERROR_REASON
35 SWITCH2_UNKNOWN_ERROR_REASON

43: TEMP_CTRL

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
2 STATE_MACHINE Error while process a state machine Line number in which the error happened
3 UNKWON_CONNECTION_TYPE Unknown connection type (Not directly nor via CAN) Value which leads to this error
4 SWITCH1_SHORT_TO_BAT_HS HV-Switch 1: Short to battery (probably on the high side) Byte 0-1: ADC value of HS_VFB Byte 2-3: ADC value of LS_VFB
5 SWITCH2_SHORT_TO_BAT_HS HV-Switch 2: Short to battery (probably on the high side) Byte 0-1: ADC value of HS_VFB Byte 2-3: ADC value of LS_VFB
6 SWITCH1_SHORT_TO_BAT_LS
7 SWITCH2_SHORT_TO_BAT_LS
8 SWITCH1_OPEN_LOAD
9 SWITCH2_OPEN_LOAD
10 SWITCH1_SHORT_TO_GND_HS
11 SWITCH2_SHORT_TO_GND_HS
12 SWITCH1_SHORT_TO_GND_LS
13 SWITCH2_SHORT_TO_GND_LS
14 SWITCH1_DIAG_DEFECT_HS
15 SWITCH2_DIAG_DEFECT_HS
16 SWITCH1_NO_POWER_SUPPLY
17 SWITCH2_NO_POWER_SUPPLY
18 SWITCH1_FS0B_NOT_RELEASED
19 SWITCH2_FS0B_NOT_RELEASED
20 SWITCH1_SBC_COM_ERROR
21 SWITCH2_SBC_COM_ERROR
22 SWITCH1_OVER_LOAD
23 SWITCH2_OVER_LOAD
24 SWITCH1_STATE_COMBINATION
25 SWITCH2_STATE_COMBINATION
26 SWITCH1_WELDED
27 SWITCH2_WELDED
28 SWITCH1_REPORTED

44: ADC_IF

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 STATEMACHINE Error while process a state machine State which leads to this error
2 PROCESS Start next ADC conversion before the previous is finished

0 = ADC 0

1 = ADC 1

45: PIN_IF

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened

46: PWM_IF

Reason ID Reason Description Additional Data
0 ASSERT Execution disrupted from assert Line number in which the assert happened
1 WRONG_DUTY_CYCLE_MEASURED Wrong duty cycle (or frequency) measured Measured duty cycle
2 WRONG_FREQUENCY_SET Invalid duty cycle set Frequency to be set
3 WRONG_DUTY_CYCLE_SET Invalid duty cycle set Duty cycle to be set

47: CMS_COM

Reason ID Reason Description Additional Data
0 ASSERT Execution disrupted from assert Line number in which the assert happened
1 MAILBOX_FULL Tx mailbox is full, sending not possible CAN message ID which can't be sent
2 SEND_EMPTY_MSG Try to send an empty CAN message CAN ID of the empty message to be sent
3 CAN_ERROR_HAPPENED CAN controller reports error Content of CAN error and status register 1 (ESR1)

48: DIAGNOSTIC_COM

Reason ID Reason Description Additional Data
0 ASSERT Execution disrupted from assert Line number in which the assert happened
1 MAILBOX_FULL Tx mailbox is full, sending not possible CAN message ID which can't be sent
2 SEND_EMPTY_MSG Try to send an empty CAN message CAN ID of the empty message to be sent

49: VCU_COM

Reason ID Reason Description Additional Data
0 ASSERT Execution disrupted from assert Line number in which the assert happened
1 MAILBOX_FULL Tx mailbox is full, sending not possible CAN message ID which can't be sent
2 SEND_EMPTY_MSG Try to send an empty CAN message CAN ID of the empty message to be sent
3 CAN_ERROR_HAPPENED CAN controller reports error Content of CAN error and status register 1 (ESR1)

50: APP_CRG_CTRL

Reason ID Reason Description Additional Data
0 ASSERT Execution disrupted from assert Line number in which the assert happened
1 WELDING_BY_SEQ_DENIED Start of "welding detection by sequence" denied -
2 SWITCH_WELDED At least one contactor is welded -
8 PARAMETER_ERROR_REDPWR_TEMPERATURE Reduce power Parameter mismatch Min Value > Max Value. none

51: ADC_CFG

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened

52: FTM_CFG

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened

53: PWM_CFG

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened

54: PILOT_CTRL

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 FREQUENCY Frequency out of range Measured frequency
2 UNKNOWN_INLET Incorrect inlet type parameterized Inlet type which leads to this error
3 PP_DECTECTION_ERROR PP resistor is in invalid range

Byte 0-1: ADC value of PP_CFB

Byte 2-3: ADC value of PP_VFB

4 DUTY_CYCLE Duty cycle out of range Measured duty cycle
5 SELFTEST_FAILED PP Self test failed (values not low in case of disabled)

Byte 0-1: Measured ADC current at PP

Byte 2-3: Measured ADC voltage at PP

6 CP_INVALID_VFB No valid ADC values for CP_VFB CP_VFB
7 CP_VOLTAGE_OUT_RANGE CP voltage out of range CP_VFB
8 PP_ADC_INVALID No valid ADC values for PP_VFB or PP_CFB

Byte 0-1: ADC value of PP_CFB

Byte 2-3: ADC value of PP_VFB

9 OPEN_LOAD

ProximityPilot: Open load was detected.

PP_VFB is smaller then PP_CFB. This is an indicator that the PP resistor is not connected.

Byte 0-1: ADC value of PP_CFB

Byte 2-3: ADC value of PP_VFB

55: PAR_IF_APP

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 STRUCT The parameter structures of the application and NVM are not compatible Hash of the parameter set stored in EEPROM
2 CHECKSUM Parameter checksum is bad Calculated checksum
3 STAY_IN_BL "Stay in bootloader" flag can't be set -
4 SET_QUALI_OPERATION_STATE Error while writing quali operation state to EEPROM -
5 RANGE_CHECK_FAILED

Parameter range check failed.

At least one parameter is not in range:

- Boolean is not true or false

- Enum is larger as its last enum value

- Integer is smaller as minimum value or larger as maximum value

Byte 0: Last boolean parameter which failed

Byte 1: Last enum parameter which failed

Byte 2: Last signed integer parameter which failed

Byte 3: Last unsigned integer parameter which failed

6 WRITE_DEFAULT_PARAMETER Default parameter set can't be written to EEPROM -

56: BTN_CTRL

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 NO_ERROR No error; should not be reported -
2 STATE_MACHINE Programming failure in state machine State which leads to this error
3 PARMAETER_BTNTYPE_INVALID Programming failure in btnCtrl_DetermineButtonState Button type which leads to this error
4 PARAMETER_OVERLAP Parameter ranges overlap, therefore no detection of the button possible -
5 PARAMETER_OUT_OF_RANGE Parameter out of range, therefore no detection of open load, short to ground possible -
6 PARAMETER_LOW_GREATER_HIGH Parameter low > high -
7 OPEN_LOAD Open load detected ADC value of BTN_VFB
8 SHORT_TO_GROUND Short circuit to ground detected ADC value of BTN_VFB
9 OUT_OF_RANGE Measured values out of range / invalid ADC value of BTN_VFB
10 SENSOR_MALFUNCTION Button sensor malfunction detected VFB as ADC value

57: DEBOUNCED_PIN_IF

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened

58: MAIN

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 NO_ERROR Cycle time was exceeded Time which leads to this error
2 STATE_MACHINE OsTasks_Input was not called -
3 PROCESS_NOT_CALLED OsTasks_Process was not called -
4 OUTPUT_NOT_CALLED OsTasks_Output was not called -
5 WRONG_HW_DETECTED Wrong hardware (e.g. B-Sample) detected Detected hardware (numerical representation)

59: SAFETY_CTRL

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 STATE_MACHINE Programming failure in state machine State which leads to this error
2 RESET_TYPE_NOT_SUPPORTED UDS Reset type not supported Value of reset type
3 E2E_PROTECTION_PARAM_INVALID E2E Protection parameter error -
4 E2E_PROTECTION_CRC_WRONG E2E Protection: checksum wrong

Byte 0: received checksum

Byte 1: calculated checksum

5 E2E_PROTECTION_SEQ_WRONG E2E Protection: sequence counter wrong

Byte 0: received sequence counter

Byte 1: previous sequence counter

60: AVG_ADC_IF

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 UNABLE_TO_MEASURE_CP_VOLTAGE Although a CP signal was detected, it was not possible to measure it. -

61: RTV

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened

62: CRG_COM

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 MAILBOX_FULL Tx mailbox is full, sending not possible CAN message ID which can't be sent
2 SEND_EMPTY_MSG Try to send an empty CAN message CAN ID of the empty message to be sent
3 CAN_ERROR_HAPPENED CAN controller reports error Content of CAN error and status register 1 (ESR1)

63: DIAGNOSTIC_COM_CMS

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 MAILBOX_FULL Tx mailbox is full, sending not possible CAN message ID which can't be sent
2 SEND_EMPTY_MSG Try to send an empty CAN message CAN ID of the empty message to be sent

64: SHB

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 OPEN_LOAD Open load between Motor+ Motor- Read error status
2 SHORT_TO_GND_OUTPUT_1 Short to GND Motor+ Read error status
3 SHORT_TO_GND_OUTPUT_2 Short to GND Motor- Read error status
4 SHORT_TO_POWER_OUTPUT_1 Short to BAT Motor+ Read error status
5 SHORT_TO_POWER_OUTPUT_2 Short to BAT Motor- Read error status
6 VPWR_OVERVOLTAGE VPWR over voltage Read error status
7 VPWR_UNDERVOLTAGE VPWR undervoltage Read error status
8 CHARGE_PUMP_UNDERVOTALGE Charge pump undervoltage Read error status
9 SPI_FRAMING_ERROR SPI framing error Read error status
10 OVERCURRENT Overcurrent Read error status
11 THERMAL_WARNING Thermal warning Read error status
12 OVERTEMPERATURE_SHUTDOWN Overtemperature shutdown Read error status
13 SPI_ERROR Error while SPI communication with SHB Status which leads to this error
14 STATE_MACHINE Error processing a state machine State which leads to this error

65: PLATFORM_IF

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 CL30_OVER_VOLTAGE CL30 over voltage CL30 ADC VFB
2 CL30_CRITICAL_OVER_VOLTAGE CL30 critical over voltage that can damage HW CL30 ADC VFB
3 CL30_UNDER_VOLTAGE CL30 under voltage CL30 ADC VFB
4 CL30_OVER_CURRENT CL30 over current CL30 ADC VFB
5 HMI_SUPPLY Internal power distribution detected an error at HMISupply output -
6 SENSOR_SUPPLY Internal power distribution detected an error at SenosorSupply output -
7 POWER_SUPPLY Internal power distribution detected an error for internal supply -
8 SBC_OVER_TEMPERATURE Over temperature of SBC SBC temperature [°C]
9 NTC_OVER_TEMPERATURE Over temperature NTC NTC temperature [°C]
10 HW_CODE_INVALID Not supported hardware Measured hardware code resistor value
11 RESTART_MCU_FAILED Restart of microcontroller via SBC auto wake-up failed SPI response code (status_t)
12 ADC_CONVERSION_TIMEOUT HWCode_VFB ADC conversion timeout. -

66: QUALI

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 TEMP1_OUT_OF_RANGE Temperature Value out or Range Actually measured temperature
2 TEMP2_OUT_OF_RANGE Temperature Value out or Range Actually measured temperature
3 TEMP3_OUT_OF_RANGE Temperature Value out or Range Actually measured temperature
4 TEMP4_OUT_OF_RANGE Temperature Value out or Range Actually measured temperature
5 PP_OUT_OF_RANGE Temperature Value out or Range PP state
6 BTN_OUT_OF_RANGE Temperature Value out or Range Button state
7 PLC_ERROR CMS PLC CAN error CMS error number except 0, 1, 5 (always active with multiple PLCs)
8 SELFTEST_INTERRUPT Selftest execution was interrupted Index of last executed test.
9 SELFTEST_FAILED At least one selftest test failed Index of last executed test
10 SELFTEST_RANGE Selftest called with wrong range. -
11 SELFTEST_STIMULATED Selftest found successful stimulation but stimulation is disabled. Index of last executed test
12 IL1_CFB_OUT_OF_RANGE Interlock 1 CFB measurement out of range for active or inactive state Actual ADC value
13 IL1_VFB_OUT_OF_RANGE Interlock 1 VFB measurement out of range for active or inactive state Actual ADC value
14 IL2_CFB_OUT_OF_RANGE Interlock 2 CFB measurement out of range for active or inactive state Actual ADC value
15 IL2_VFB_OUT_OF_RANGE Interlock 2 VFB measurement out of range for active or inactive state Actual ADC value
16 SM_TIMEOUT State machine timeout code line of occurrence
17 CHARGE_CAN Charging CAN communication error actual received value
18 LED_ERROR LED Status error

Byte 0: Status LEDCTRL_TPS92518_LED_3_4

Byte 1: Status LEDCTRL_TPS92518_LED_1_2

19 TEMP1_STATUS_NOK Temperature sensor 1 status is not ok Error reason (see TempCtrl_Status_t)
20 TEMP2_STATUS_NOK Temperature sensor 2 status is not ok Error reason (see TempCtrl_Status_t)
21 TEMP3_STATUS_NOK Temperature sensor 3 status is not ok Error reason (see TempCtrl_Status_t)
22 TEMP4_STATUS_NOK Temperature sensor 4 status is not ok Error reason (see TempCtrl_Status_t)

67: STACK_MONITOR

Reason ID Reason Description Additional Data
0 STACK_UNDERFLOW A stack underflow was detected -
1 STACK_OVERFLOW A stack overflow was detected -

68: IRQ_MONITOR

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 ADC0 Interrupt handler for ADC0 was called unintentionally. -
2 ADC1 Interrupt handler for ADC1 was called unintentionally. -
3 CAN0_WARNING Interrupt handler for CAN0 (bus off, Tx/Rx warning) was called unintentionally. -
4 CAN0_ERROR Interrupt handler for CAN0 (Error) was called unintentionally. -
5 CAN0_WAKE_UP Interrupt handler for CAN0 (WakeUp) was called unintentionally. -
6 CAN0_0_15_MB Interrupt handler for CAN0 (Mailbox 0 ... 15) was called unintentionally. -
7 CAN0_16_31_MB Interrupt handler for CAN0 (Mailbox 16 ... 31) was called unintentionally. -
8 CAN1_WARNING Interrupt handler for CAN1 (bus off, Tx/Rx warning) was called unintentionally. -
9 CAN1_ERROR Interrupt handler for CAN1 (Error) was called unintentionally. -
10 CAN1_0_15_MB Interrupt handler for CAN1 (Mailbox 0 ... 15) was called unintentionally. -
11 CAN1_16_31_MB Interrupt handler for CAN1 (Mailbox 16 ... 31) was called unintentionally. -
12 CAN2_WARNING Interrupt handler for CAN2 (bus off, Tx/Rx warning) was called unintentionally. -
13 CAN2_ERROR Interrupt handler for CAN2 (Error) was called unintentionally. -
14 CAN2_0_15_MB Interrupt handler for CAN2 (Mailbox 0 ... 15) was called unintentionally. -
15 FTM2_CH2_CH3 Interrupt handler for FTM2 Channel2/3 was called unintentionally. -
16 ADC0_SEQUENCE ADC0: Problem with the conversion sequence in this conversion group

Byte 0: Index of the conversion group

Byte 1: Enable channel mask

Byte 2: Complete channel mask

Byte 3: Error channel mask

17 ADC1_SEQUENCE ADC1: Problem with the conversion sequence in this conversion group

Byte 0: Index of the conversion group

Byte 1: Enable channel mask

Byte 2: Complete channel mask

Byte 3: Error channel mask

18 ADC0_STATUS ADC0: Error in status register SC2 Content of ADC.SC2
19 ADC1_STATUS ADC1: Error in status register SC2 Content of ADC.SC2
20 ADC0_COCO ADC0: A conversion complete flag of a configured ADC channel is not set

Byte 0: Conversion group

Byte 1: Index of configured channel

21 ADC1_COCO ADC1: A conversion complete flag of a configured ADC channel is not set

Byte 0: Conversion group

Byte 1: Index of configured channel

22 NMI_FAULT NMI fault Content of the Configurable Fault Status Register
23 HARD_FAULT Hard fault Content of Hard Fault Status Register
24 MEMORY_MANAGEMENT Memory Management fault Address causing the bus MemManage fault
25 BUS_FAULT Bus fault Address causing the bus fault
26 USAGE_FAULT Usage fault Content of the Configurable Fault Status Register
27 ERM_DOUBLE_FAULT ECC fault in SRAM_L or SRAM_U (ERM ECC double bit fault) Address where the ECC fault happened 0xFFFFFFFF = Fault address can't be determined.
28 UNUSED_INTERRUPT Unused Interrupt executed Interrupt number
29 FTFC_DOUBLE_FAULT FTFC ECC double bit fault -
30 MPU_FAULT MPU detected an address violation The address causing the violation
31 UNKNOWN_BUS_FAULT Bus fault happened but reason is unknown -

69: SPI

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 SLEEP_WAKE SPI driver returned an error in module sleep wake

Byte 0 ... 1: Status of SPI communication (status_t)

Byte 2 ... 3: Line number in which the error was reported

70: INTERLOCKCTRL

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 IL1_MALFUNCTION Malfunction of the interlock 1 circuit

Byte 0-1: Measured CFB

Byte 2-3: Measured VFB

2 IL2_MALFUNCTION Malfunction of the interlock 2 circuit

Byte 0-1: Measured CFB

Byte 2-3: Measured VFB

3 IL1_S2BAT Open load or short to battery detected at il1

Byte 0-1: Measured CFB

Byte 2-3: Measured VFB

4 IL2_S2BAT Open load or short to battery detected at il2

Byte 0-1: Measured CFB

Byte 2-3: Measured VFB

5 IL1_S2GND Short to GND detected at il1

Byte 0-1: Measured CFB

Byte 2-3: Measured VFB

6 IL2_S2GND Short to GND detected at il2

Byte 0-1: Measured CFB

Byte 2-3: Measured VFB

7 IL1_OUT_OF_RANGE Measured resistor is out of range at il1 Measured resistor value
8 IL2_OUT_OF_RANGE Measured resistor is out of range at il2 Measured resistor value
9 IL2_CROSSCONNECTION Cross connection detected

Byte 0-1: Measured CFB

Byte 2-3: Measured VFB

10 SEQUENCE_STATE_ERROR Invalid interlock sequence state -

71: TPS92518

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 LED_1_BOOTUV_ERROR Under voltage reported by TPS92518. Also signals an open load. Which chip was selected
2 LED_2_BOOTUV_ERROR Under voltage reported by TPS92518. Also signals an open load. Which chip was selected
3 THERMAL_WARNING Thermal warning reported by TPS92518 Which chip was selected
4 SPI_FRAME_ERROR SPI frame error reported by TPS92518 Which chip was selected
5 POWER_CYCLED Power cycle occurred since last read of the status register Which chip was selected
6 SPI SPI driver returned an error in module Tps92518If Line number in which the error was reported

72: CORE_MONITOR

Reason ID Reason Description Additional Data
0 INTERRUPTED Selftest execution was interrupted
1 FAILED At least one selftest test failed
2 RANGE Selftest called with wrong range.
3 STIMULATED Selftest found successful stimulation but stimulation is disabled.
4 NVIC_ERROR Restore of NVIC registers didn't happened Index of last executed test.

73: ADC_MONITOR

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 BANDGAP_ADC0 Bandgap voltage measured by ADC0 is out of range ADC value of bandgap
2 BANDGAP_ADC1 Bandgap voltage measured by ADC1 is out of range ADC value of bandgap
3 VREF_HIGH VRefH voltage is out of range ADC value of VRefH
4 VREF_LOW VRefL voltage is out of range ADC value of VRefL
5 START_UP_CHECK_NOT_EXECUTED Start up check not executed Status of the start up check
6 START_UP_CHECK_VREFH_FAILED_1 VRefH voltage in start up test is to low ADC value of VRefH
7 START_UP_CHECK_VREFH_FAILED_2 VRefH voltage in start up test is to low ADC value of VRefH
8 START_UP_CHECK_VREFL_FAILED_1 VRefL voltage in start up test is to high ADC value of VRefL
9 START_UP_CHECK_VREFL_FAILED_2 VRefL voltage in start up test is to high ADC value of VRefL
10 START_UP_CHECK_EXT_REF_FAILED_1 CL30_VFB voltage in start up test is out of range ADC value of CL30_VFB
11 START_UP_CHECK_EXT_REF_FAILED_2 CL30_VFB voltage in start up test is out of range ADC value of CL30_VFB

74: REG_MONITOR

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 WRONG_REG_VALUE A register has a wrong value Address of the register with wrong value
2 WRONG_REG_VALUE_ADDITIONALDATA Extension of the error entry WRONG_REG_VALUE. Content of the register with the pale values.

75: SAFETY_SUPERVISOR

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 BOOTLOADER_INCOMPATIBLE Bootloader and firmware versions are incompatible First 4 byte of the git hash of the incompatible bootloader

76: ECC_MONITOR

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 RAM_ONE_BIT_ERROR Test for one-bit errors in RAM failed Byte 0: detected error event (0 = None, 1 = one-bit, 2 = two-bit)
2 RAM_ONE_BIT_ADDRESS Location of one-bit error in RAM is wrong Address / location, where the one-bit error happened
3 RAM_TWO_BIT_ERROR Test for two-bit errors in RAM failed

Byte 0: detected error event (0 = None, 1 = one-bit, 2 = two-bit)

Byte 1: boolean flag, if the two-bit error ISR was called

4 RAM_TWO_BIT_ADDRESS Location of two-bit error in RAM is wrong Address / location, where the two-bit error happened
5 FLASH_TWO_BIT_ERROR Test for two-bit errors in flash failed -

77: CLOCK_MONITOR

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 PLL_FREQUENCY_ERROR PLL frequency test detected an error FTM1 value after overflow of FTM4

78: MPU_MONITOR

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 ERROR_INIT Initialization of the MPU failed Error status
2 ERROR_INSIDE_START MPU test "inside start address" failed Checked address
3 ERROR_INSIDE_END MPU test "inside end address" failed Checked address
4 ERROR_OUTSIDE_START MPU test "outside start address" failed Checked address
5 ERROR_OUTSIDE_END MPU test "outside end address" failed Checked address

79: IVT

Reason ID Reason Description Additional Data
0 ASSERT Used by the assert function Line number in which the assert happened
1 INVALID_WIRING_PARAMETER IVT-S wiring parameter is invalid Set invalid value
2 PARAMETER_ERROR_NO_CHARGING_CAN_AVAILABLE One of the following parameters is set to charging CAN on a Hardware without one: PAR_VehicleVoltageSource, PAR_InletVoltageSource, PAR_ChargingCurrentSource -
3 ERROR Either the IVT reported an error for the last 100ms or we didn't received messages.

Byte 0: Measurement which leads to the error ( 0 = Current, 1 = InletVoltage, 2 = VehicleVoltage, 3 = Temperature )

Byte 1: Error status send by IVT

bit 0: set if OCS is true

bit 1: set if - this result is out of (spec-) range,

- this result has reduced precision - this result has a measurement-error

bit 2: set if

- any result has a measurement-error

bit 3: set if

- system-error, sensor functionality is not ensured!

4 PARAMETER_ERROR_CHARGING_CAN_BITRATE_NOT_CONFIGURED Charging CAN bitrate is configured as SNA while IVT is configured on Charging CAN. -



 


CHARX help
Published/reviewed: 2026-02-23,, Version history