Safety Information

Identification of warning notes

 

warning signThis symbol indicates hazards that could lead to personal injury. 

There are three signal words indicating the severity of a potential injury.

DANGER

Indicates a hazard with a high risk level. If this hazardous situation is not avoided, it will result in death or serious injury.

WARNING

Indicates a hazard with a medium risk level. If this hazardous situation is not avoided, it could result in death or serious injury.

CAUTION

Indicates a hazard with a low risk level. If this hazardous situation is not avoided, it could result in minor or moderate injury.

 

warning sign

This symbol together with the NOTE signal word warns the reader of actions that might cause property damage or a malfunction.

 

warning sign

Here you will find additional information or detailed sources of information.

 

Qualification of users

 

The use of products described in this user manual is oriented exclusively to:

  • Electrically skilled persons or persons instructed by them. The users must be familiar with the relevant safety concepts of automation technology as well as applicable standards and other regulations.
  • Qualified application programmers and software engineers. The users must be familiar with the relevant safety concepts of automation technology as well as applicable standards and other regulations.

 

Security in the network

 

damage or a malfunction sign

Connecting devices to a network via Ethernet always entails the risk of unauthorized access to the network. 

 

Therefore, please check for the option of disabling active communication channels in your application (e.g., FTP, DCP, HTTP, HTTPS, etc.) or setting passwords to prevent third parties from accessing the controller without authorization and modifying the system.

 

Due to its communication interfaces, the controller should not be used in safety-critical applications unless additional security appliances are used. Please take additional
protective measures in accordance with the IT security requirements and the standards applicable to your application (e.g., virtual networks (VPNs) for remote maintenance access, firewalls, etc.) for protection against unauthorized network access.

 

On first request, you shall release Phoenix Contact and the companies associated with Phoenix Contact GmbH & Co. KG, Flachsmarktstraße 8, 32825 Blomberg, Germany in accordance with §§ 15 ff AktG (German Stock Corporation Act), hereinafter collectively referred to as “Phoenix Contact”, from all third-party claims made due to improper use.


For the protection of networks for remote maintenance via VPN, Phoenix Contact offers the mGuard product range of security appliances, a description of which is provided in the latest Phoenix Contact catalog (phoenixcontact.net/products).

 

Additional measures for protection against unauthorized network access can be found in the AH EN INDUSTRIAL SECURITY application note. The application note can be downloaded at phoenixcontact.net/product/2404267.

 

Intended use

 

CAPAROC is a modular circuit breaker system. The devices correspond to protection class IP20. They are intended for use in closed control cabinets or control boxes (junction boxes) with IP54 degree of protection or higher.


The devices are designed for use in industrial environments.

 

Product changes

 

Modifications to the device hardware are not permitted. Modifications to the firmware are only permitted by means of firmware updates provided by Phoenix Contact.

 

Incorrect operation or modifications to the device can endanger your safety or damage the device. Do not repair the device yourself. If the device is defective, please contact Phoenix Contact.

 


CAPAROC online documentation
Published/reviewed: 2025-08-18, en revision 000, Version history