W e are constantly surrounded by direct voltage in everyday life. “Every electrical device that has a display uses direct current – from washing machines and smartphones to car electronics. Fundamentally, every electric drive uses direct current and every battery stores direct current. There are very few appliances, such as old toasters and clothes irons, that directly use alternating current”, explains Martin Wetter. Christian Helmig adds, “With the advent of renewable energy generators, especially solar, direct voltage has become a big issue again. Whether in solar panels or wind turbines, the captured energy is first converted into direct current. And in electric vehicles, batteries with direct current drive the wheels”. Both engineers are graduates of the Dortmund Institute of High Voltage Engineering, where they also completed their doctorates and worked together. Wetter, hailing from Münster in Germany, was drawn to Blomberg in East Westphalia way back in 1997. For a long time, he managed the world-renowned Trabtech overvoltage laboratory on the Phoenix Contact campus and is now responsible for the core business of Power Reliability. Helmig, a native of Westphalia, followed on five years later and is now Head of the Field Device Connectors unit in the Device Connection Technology division. Advantage direct current There are tangible arguments that play into the hands of Thomas Alva Edison’s upcoming successors: efficiency, storability, and resources. It is immediately obvious that with every transformation of energy, part of it is lost as heat. When electricity is generated by wind or the sun, it is initially available as DC voltage. The conversion to alternating current “eats up” around 20 percent of the original energy. This can be saved if direct current is used immediately as it is. The second advantage is recuperation, i.e., the use of excess kinetic energy. “This is particularly easy with direct current. This is not only important for e-mobility but also in many industrial areas, such as high-bay warehousing cables required have significantly smaller cross-sections. And the required connected load, i.e., the amount of electrical energy that the grid operator contractually provides, can be around two-thirds lower than with a conventional AC connection. “This immediately saves money, even before a machine runs”, explains Christian Helmig. Advantage alternating current The advantages of alternating current come into play in terms of long-distance power transmission. Dr. Wetter explains, “If I want to transmit a certain amount of power, I need current multiplied by voltage. If I want to transmit a lot of power, I have to increase the current or voltage The three DC trump cards Efficiency Energy savings of around 20 percent can be achieved by using direct current Storability Direct current is the energy form of battery technologies. This makes electricity directly storable Resources In addition to efficiency, direct current saves materials due to lower copper thicknesses systems and industrial robots. Energy is recovered when or both. However, the transmission losses along such the movement is reduced”, adds the Innovation Manager, Wetter. “Efficiency is therefore one of the central issues when it comes to increasing the use of direct current.” lines depend solely on the current. In fact, they increase quadratically, which means that twice the current equals four times the losses. This is why we transmit high The ability to store it directly is another advantage. powers over long distances using alternating current Energy from batteries is direct current. Direct current with high voltages. It minimizes the transmission losses. systems can store and retrieve energy directly in batteries The conversion is simple and extremely reliable with without conversion. The complexity of the systems is decreased, which in turn leads to increased efficiency. the appropriate transformers”. Alternating current has therefore become standard in the classic technology of The next advantage is the conservation of resources, which begins with saving material, because the copper distribution grids with a few large power stations and a star-configuration distribution grid. → The Phoenix Contact innovation magazine UPDATE 21