Targeted thermal management The power density of electronic systems increases as their size decreases. This trend makes it a challenge to dissipate the lost heat into the environment in a targeted manner. To describe the thermal conduction in electronic components, the thermal resistance Rth in K/W is used. This value describes the maximum heat output P [W] that can be dissipated with a specified temperature difference ΔT [K], and serves as an indicator of the performance of a heatsink. Heat can be transferred through thermal conduction, convection, and heat radiation. When developing a cooling concept, analyzing the heat paths and higher-level transport mechanisms is particularly challenging. Through targeted optimization of the heat transport mechanisms, the dissipation performance is increased and, at the same time, the service life of the electronic components is extended. Phoenix Contact 7