Photovoltaics Data networking is playing an ever increasing role in photovoltaic systems. Due to the decentral structure in ground- mounted systems, transmission systems are particularly exposed to the dangers of coupled, transient overvoltages. Sensors, data loggers, and transmission systems ensure the comprehensive, split- second recording of PV performance data and meteorological measured values. Permanent availability is prerequisite for the stable operation of such a system. It is necessary to use special surge protection products to protect the copper-based transmission systems against transient Railway infrastructure Control command and signaling technology ensures safe and reliable railway operations. In signal boxes, secured routes are set up, points are set, and the corresponding signals are switched. In addition to signals, external signal technology systems also contain components such as axle counters and track-clear signaling devices, which are necessary for interference-free operation. Overvoltages that are caused by lightning strikes or sparkovers on overhead lines, for example, can occur at any time in the extensive rail network and endanger the measurement and control data. Transportation infrastructure Transient overvoltages caused by lightning strikes or switching operations can damage technical systems and devices, and even cause them to fail. Despite their underground location, tunnels are not protected against such events. There are numerous safety-relevant systems in a tunnel, such as ventilation, emergency lighting, and traffic signal control, and it is essential to ensure that they operate reliably. Any failures that arise due to overvoltage will lead to expensive repairs and even tunnel closure. Each interface therefore requires suitable surge protection. surge voltages during storms. In the worst case, a transient overvoltage can cause a complete failure of the system monitoring system if control and data cables are unprotected. Depending on requirements, our comprehensive portfolio includes the perfect surge protective devices to protect measurement, control, and data cables in photovoltaic projects. Reliable lightning and surge protection is therefore essential to protect signal technology and control systems from damage caused by transient couplings. Since high signal voltages are often used in railway technology, the CLIXTRAB product family of surge protective devices offers optimal protection even for these special requirements. The extensive product range features the right solution for every requirement, such as for fast data communication or for monitoring and controlling technical systems. Intelligent components detect when their performance limit has been reached at an early stage so that the protective device can be replaced and tunnel operation remains interference-free. l y g o o n h c e t l o r t n o c d n a t n e m e r u s a e m r o f n o i t c e t o r p e g r u S Prevention of complete PV facility failures Modern railway infrastructure with surge protection Safely through the tunnel thanks to surge protection Phoenix Contact 51