Directives and standards for lightning and surge protection for photovoltaic rooftop systems If signal and communication circuits are present in the photovoltaic system in question, these should also be equipped with surge protective devices. ❯ For the appropriate products for MCR and data lines, see page 23. When planning and installing new photovoltaic systems in Germany, it is important to comply with certain requirements. This applies not only to the systems themselves, but also to the surge protection of the corresponding system parts. DIN VDE 0100-712 describes how to plan and install photovoltaic systems in Germany. In order to optimally protect the systems against the effects of surge voltages, it is also important to ensure that the correct type of surge protection is used. On the alternating current side (AC side), surge protection is required in accordance with DIN VDE 0100-443. If the protection of the inverter is to be ensured, protection is also required on the direct current side (DC side) in accordance with DIN EN 62305-3 Supplement 5. AC side: Protective measures in the main distribution DIN VDE 0100-443 and DIN VDE 0100-534 specify whether and, if necessary, which surge protection measures must be provided on the AC side of the photovoltaic power supply system. DC side: Protection of the photovoltaic power supply system If it proves necessary to protect the inverter, DIN EN 62305-3 Supplement 5 stipulates that surge protective devices must primarily be installed in the proximity of the PV panels (DC 1). Additional protective measures may be necessary in the proximity of the inverter in the case of long cable lengths (> 10 m, DC 2). Protection of the inverter Do you have further questions about the normative principles or are you about to embark on a project and need advice? Then contact our experts for surge protection quickly and easily via WhatsApp. • Use the number +49 5235 343654 • Scan the QR code 4 Phoenix Contact