SOLAR POWER IT systems everywhere, which they use to provide monitoring right down to module level via the inverters. This is not a problem in a new solar park. But retrofitting existing systems is a problem because the insulation marketers, who are active on the electricity exchange, all regulate within a time window of 15 minutes. When the exchange prices are really good, the participating park operators can, for example, feed in fully for 15 minutes. material, which has been buried in the ground for years, However, if this reverses and prices fall, the order is given ages and can become brittle. We therefore want to extend not to feed anything into the grid for 15 minutes, or to the substation’s monitoring relay so that we can keep track store the electricity in the battery storage system. Due to of this material’s condition and issue an early warning. the often unsatisfactory internet coverage in Germany, In addition, when the miniature circuit breaker trips, we though, it can happen that the internet is completely want to be able to differentiate whether this was caused by disconnected for control commands and these control a subordinate protection circuit tripping due to frequency commands come to nothing. This quickly leads to or voltage or by an actual insulation event”. considerable contractual penalties, which can quickly run Transparent grid The self-confident industrialist is also passionate about another issue: the lack of transparency regarding the energy grid operators’ curtailment measures. “For the park operators, this means a loss of earnings of many thousands of euros, often even hundreds of thousands. The law stipulates that there is financial compensation for this. We now track the condition of the systems via VPN, record this in a database on our own portal, and document this for the operators. This gives us a very good overview of what is actually going on in the grid”. Marina Friedberger adds, “The aim is to record every five minutes whether the grid operator is regulating the connection. We want to export this data and make it available to the solar park operator. At the end of the day, they know what they really should have earned and are able to take this up with the grid operator. We developed the interface that we use for this based on the power control unit’s PLCnext Technology”. “This transparency was initially very surprising for the power providers”, Josef Ecker continues. This gives the Josef Ecker, Marina Friedberger, and Helmut Schratzenstaller (from left) residents of Landshut and their customers unprecedented insights into the architecture of the power supply, as Helmut Schratzenstaller confirms: “We repeatedly see that on a beautiful sunny day in Germany, around 30 to 40 percent of the systems are being derated. And this varies greatly from grid operator to grid operator”. Electricity as a commodity While the man from Landshut and his team are causing into five-figure sums. For 15 minutes of incorrect feeding! Of course, no park operator can risk that". “We are therefore working on solutions to equip the substations with Starlink modules from the start so that they are reliably real-time capable”, says Josef Ecker, outlining the next challenges. “Compared to the potential contractual penalties, the costs for the satellite network quite a stir on the operator side, he is already devoting are peanuts”. himself to completely new tasks: ”Our next big topic is battery storage systems. Technically, they operate with a different control method based on the frequencies The solutions that Elektro Ecker is developing here on the basis of feed-in controllers from Phoenix Contact are of great interest for the entire German power grid. We can in the power grid. The operators of these utility-scale storage facilities have a very different view of power grids. therefore look forward to the next news from the farm near Landshut. (lo) This is where the direct marketers come in”. Helmut Schratzenstaller explains the new outlook: “The direct elektroecker.de (German only) The Phoenix Contact innovation magazine 19