The basics of device circuit breakers | Differences between the technologies system controller. If an event occurs, it is detected immediately and reported. This approach reduces the period of any voltage dip to a minimum. Despite the event, the system voltage remains stable. In the event of overload current or a short circuit, the devices are promptly switched off. Electronic circuit breakers are in some cases equipped with active current limiting. This function limits the short circuit and overload currents, depending on the product range, to a value of 1.25 to 2 times the nominal current. This protects the power supply against currents that are too high and prevents the output voltage from dropping at the switched-mode power supply unit. Another benefit of this electronic technology is the ability to virtually completely plan out the connected load of any DC power supply. In addition, longer cable paths between the power supply and load are possible without negatively impacting the shutdown behavior. Tripping characteristics and dynamics Thanks to intelligent current analysis, modern electronic circuit breakers can differentiate between many different operating and failure scenarios. The result is a dynamic in the characteristic curve. This means that any fault-related shutdown is not dependent solely on current and time. The load and power supply are detected, optimizing the startup process. In this way, the operation of the electronic protection is illustrated in a dynamic characteristic curve. Similar to traditional fuses, this is also done by defining an overload and short-circuit range. Some electronic circuit breakers have different characteristic curves. The purpose of these differences is first and foremost to offer the user familiar selection options. However, it is not necessary to differentiate 14 PHOENIX CONTACT s , t 100 10 1 0,1 0,01 0,001 1 2 4 8 x In 16 32 64 Fig. 16: Short-circuit behavior and dynamic overload detection range When it comes to burn-through fuses and thermomagnetic circuit breakers, the different characteristic curves are known, such as fast-acting, medium blow, or slow blow. A modern electronic protective device with intelligent short-circuit detection and dynamic overload behavior is replacing the wide range of characteristics mentioned above. among different characteristic curves. As opposed to thermal or thermomagnetic fuses, the electronics in modern electronic circuit breakers react dynamically. Figure 16 shows the various ranges: 1. Short circuit behavior (green line): If a short circuit is detected, the fault is immediately shut down. To prevent any negative impact on the loads, this has to happen without a time delay. Particularly with a PLC, a shutdown must occur within 10 ms (see also controller standard, p. 5). 2. Dynamic overload detection range (blue area): Depending on the height and course of the flowing current, the intelligent detection also ensures a shutdown in the case of an overload. This process permits the overcurrent to persist for different lengths of time, depending on its progression and the stability of the supply voltage. The overload is shut down before a dangerous condition arises. Here also, the dynamics associated with electronic circuit breakers provide a critical advantage. If a fault is detected, it is shut down promptly, keeping the remaining supply in mind. Loads can be detected in this way and can be started even when high starting currents are present.