Ice detection – systems at a glance Naturally, this does not result in a particularly realistic assessment of the situation on the blade and thus, out of necessity, becomes a highly conservative interpretation of the measured values in order to avoid possible risks. Result: The system is shut down earlier to be on the safe side. And: An automatic restart is not possible, because it cannot be determined whether ice has stopped forming on the rotor blades. The advantage of nacelle-based systems is the perceived low procurement price. Blade-based ice detection Blade-based measurement systems measure ice build-ups directly on the rotor blades. Here, a distinction is made between two measurement methods: • Measurements outside, directly on the rotor blade using capacitive sensor technology, which directly detects ice and measures its thickness. • Measurements inside the blade, using fiber-optic or piezoelectric methods, with the formation of ice being calculated based on the changes in the vibration behavior of the rotor blade. There are now several ways to detect the formation of ice. The individual systems for ice detection use different technologies: • Measuring the ambient temperature • Measuring the ambient temperature and humidity • Anemometer comparisons • Optical camera systems • Changes in the power characteristic curve, for example the power output of the WTG • Measuring the ice directly on the rotor blade (vibration-based or by resistance measurement) The key is where the measurements are taken. The difference between ice forming on the rotor blade and ice forming on the nacelle is often greater than expected. Factors such as geometry, dimensions, movement, and flow velocity mean that completely different climatic influences exist on the blade that are not present at the weather mast on the nacelle. The fact that the systems listed vary greatly in their accuracy mean that they have differing influences on the yield, but also play an important role in generator safety considerations. As a result, two technical solutions in particular have become established on the market: Nacelle-based ice detection and blade-based ice detection. Nacelle-based ice detection Nacelle-based systems are, conventionally, mounted on the WTG weather mast and measure specific meteorological parameters to determine the possibility of ice accumulation. Specific technologies, such as comparing two anemometers, measuring the humidity, or ultrasonic ice detection, are used for this. Regardless of which version is used, none of them measure the ice accumulation on the rotor blade, but rather at a location where entirely different conditions prevail. 10 UPDATE SPECIAL The Phoenix Contact innovation magazine