MTP APL 5G Modular production Advanced Physical Layer Industrial 5G Modular automation plays a vital role in enabling the capacity of production plants to be adapted to market demands. Phoenix Contact will be happy to advise you regarding the implementation of NAMUR recommendation NE 148 and support you in the startup of your plant modules. We also offer the MTP Designer tool that enables you to plan modules very quickly and easily. Web code: #2265 APL was developed specifically for use in intrinsically safe areas of process technology. This enables IP-based communication through to the sensor without system breaks or gateways. The standards necessary for this technology are being developed in a collaborative project between three fieldbus organizations (Fieldcom Group, ODVA, and PI) and eleven industrial partners. Phoenix Contact is one of the initiators of this project and is also involved as an industrial partner. Working together with Quectel and Ericsson, we have developed the first industrial 5G router for local industrial applications in private 5G networks. This means that industrial applications such as machines, controllers, and other devices can now be connected to a private 5G network, allowing their coordination in terms of resource utilization, priority, and behavior. Furthermore, we are a founding partner, active participant, and member of the board of the 5G-ACIA. Web code: #2718 Web code: #2719 PLCnext Store Visit the PLCnext Store where the latest software solutions, such as protocol libraries and complete control applications, are available from Phoenix Contact and other providers. PLCnext Community In the PLCnext Community, you can exchange ideas with PLCnext Technology users and benefit from the experiences of other users. Web code: #1509 PLCnext Technology ecosystem Along with the hardware, we also provide you with a tool landscape with limitless openness – designed to elevate automation technology to a new level. PLCnext Engineer Use PLCnext Engineer, our proprietary development environment, and experience the openness of this system in the implementation of programming in oil and gas applications. These can be coded both in the classic IEC 61131 languages as well as in various high-level languages, such as C++ or C#. Moreover, Simulink, a graphic user interface based on Matlab, can be integrated into the code generation. PLCnext Control PLCnext Control devices are the PLCs for your future automation applications. The device hardware is available in various performance classes. The PLCs are characterized by the support of proven as well as future transmission standards such as OPC UA and ready-prepared cloud communication, among other features. PHOENIX CONTACT 7