T he high standards for the design of a wind turbine gen- erator and the quality-oriented manufacturing process- es, in combination with high skilled commissioning and servicing teams, enable this industry to face the growing de- mand of renewable energy and ensure a reliable energy source for the United States. Industry facts There are now nearly 60,000 wind turbines with a combined capacity of 110,000 MW operating. Over the past decade, U.S. wind power has more than tripled and has become the largest renewable energy in the country. Today, more than 120,000 U.S. workers are supporting one of the fastest-growing industries in the United States. A rapidly growing number of installed turbines scaling from 2 MW to 4 MW and an increase in rotor size from approximately 100 m to 150 m over the last 10 years have put a demand on pro- duction components and materials to help reduce the levelized cost of energy. The life expectancy of a wind turbine is about 20 years, over which it must operate reliably and safely, under haz- ardous stormy conditions. The reliable, safe, and benefi cial op- eration of these wind turbines requires additional use of smart sensors and data-monitoring devices with the right algorithmic software to detect a critical failure in an early stage to prevent or avoid a dangerous situation. Our mission As a partner in the wind industry over the last decade, Phoenix Contact developed key technologies to increase the effi ciency, safety, and security of these systems. Reliable power supplies, robust surge protection, functional safety as a standalone or controller solution, and several monitoring solutions are just a few examples of these technologies. Phoenix Contact is also working closely with technology partners like WindESCo and channel partners like Motion Industries for the retrofi tting mar- ket. The target is to provide innovative monitoring technologies and system protection upgrades to optimize existing wind tur- bines. Technical hazards Depending on the location, wind turbine generators are exposed to completely different loads. Various wind and weather situa- tions affect the operational safety and the service life of a wind turbine generator. Therefore, it is important to monitor contin- uously critical signals such as rotation speed, acceleration, wind speed/direction, and energy productions. Drivetrain vibration/ temperature, hydraulic pressure, and critical system feedbacks from the yaw, pitch, and brake system are also relevant to put the turbine during an emergency event into a fail-safe state. To ensure the safety of employees in wind turbine generators, the towers must be illuminated safely. To this end, Phoenix Con- tact offers a tower lighting system using maintenance-free LED lights. The LED lights are supplied centrally by an uninterrupt- ible power supply (UPS) installed in the tower base. Even before climbing the tower, the service technician can fi nd out the state of the UPS and the batteries. The powerful LED modules conform to international standards, and can also be used in the nacelle or hub of a wind turbine. They provide good luminous intensity even at low temperatures. The lights have a service life of 50,000 hours, so they generally do not have to be replaced. Due to the low current consumption of the LED technology, the lights also function as emergency lighting. In the event of power failure, a central battery continues to power the lights for up to 90 minutes. This will allow the service technician to exit the tower of the wind turbine generator safely. During the past decade, wind power has tripled in the U.S. 20 UPDATE 5/20 The Phoenix Contact innovation magazine