ENERGY FLOW The early planner The first contact with Enapter took place in 2022, when an initial test system with 10 stacks was constructed. This was true pioneering work, which was realized together with the Münster University of Applied Sciences and in which all parties went through a steep learning curve. This small pilot system is still used by the university for training purposes today. Because of the experience gained, Phoenix Contact was involved in the megawatt electrolyzer right from the start. In addition to the power supply, connections, and Enapter The German-Italian company is building an 82,000 square meter campus in Saerbeck near Münster, where a large part of the production, research, and development of electrolyzers will be located in the future. The man behind Enapter is Sebastian-Justus Schmidt. The then General Manager of a software company moved to Chiang Mai in Thailand in 2004. A prototype of a hydrogen electrolyzer was installed in his house there a few years later. This was the first self-sufficient apartment building in the world to be powered by a hydrogen-based energy system. Schmidt took over the Italian manufacturing company ACTA in 2017 and renamed it Enapter (“en” from energy, “apter” from adapter). Enapter is building a campus in Saerbeck, Westphalia 42 UPDATE 2/23 The Phoenix Contact innovation magazine controllers, functional safety also had to be integrated. Andreas Lautmann, a power-to-X expert at Phoenix Contact, emphasizes the importance of this early collaboration. “Our specialists set the course for a safe design-in at an early stage. If safety issues are only discovered later, during the engineering process, the project will usually take significantly longer. In developing the AEM electrolyzer, we were not just component suppliers – we also provided advice, planning, and the documentation for the safety concept”. The Business Development Manager considers this overall approach to be important and exemplary. “During the collaboration with Enapter and the Münster University of Applied Sciences, which was also a partner in this project, it became clear once again that a structured, well-documented process for design and engineering is critical for the safety of the overall system. In other words, safety is about more than just the use of certified components. This is applicable to all the relevant aspects of functional safety, explosion protection, cybersecurity, and, finally, the necessary CE marking in these systems.” Control under overpressure The control center of the system is gas-tight and separated from the process room. There is also a slight overpressure here, so that even in the event of a leak, no hydrogen can penetrate. Ayhan Birinci was project manager on the Phoenix Contact side and knows the system down to the last connector. “With the exception of a few fuses and circuit breakers, the control cabinets are equipped entirely with Phoenix Contact components. These include both real-time and safety-oriented control technology up to SIL 3. It also comprises network components, including a firewall for remote access. The operating panel and associated software were also supplied by Phoenix Contact”. The superordinate system controller was built with devices from the PLCnext product family. This controller fulfills such functions as ventilation and water pretreatment control, emergency shutdown capability, fill level monitoring, and electrolyte solution supply. Rounding out the control cabinet equipment are 24 V DC power supplies manufactured in-house as well as signal converters and connection technology for field cabling. In addition, the Phoenix Contact control cabinets were designed, documented, and produced ready-to-connect. First use with grid support For the pilot system, the energy for electrolysis is still drawn from the “normal” power grid. It is therefore necessary to convert the incoming 400 V alternating voltage. And the Phoenix Contact portfolio also had a solution for this, as →