A new dimension in the water/energy infrastructure relationship is the impact from weather and the environment. This was tragically illustrated in the aftermath of Hurricane Ida, which struck the Louisiana coast on August 29, 2021. Ida left hundreds of thousands without power as the result of serious damage to power distribution systems, and without water due to water systems crippled by power outages or flood waters. Additionally, Ida knocked out most of the Gulf of Mexico oil and gas production operations, impacting both fuel supplies and market pricing. Years before Hurricane Ida made landfall, a DOE report noted that it is time for a more integrated approach to address the challenges and opportunities of the water/ energy nexus. The All Electric Society The global community is facing what appears to be two conflicting needs — the pursuit of economic development and growth that requires the extensive use of natural resources to power infrastructure, and the mitigation of the impact on the environment from climate change to protect those resources. Both needs can be met through the concept of the “All Electric Society,” which promotes smart consumption of resources while protecting the environment. The vision of the All Electric Society (AES) is a world that can fulfill its own entire energy needs through renewable sources, and where renewably generated electrical energy is readily available and affordable where consumed. The goal of the All Electric Society is to ensure sustainable global development that raises the standard of living for all while conserving our natural resources. Water is one such resource. The United Nations’ 17 Sustainable Development Goals (SDGs) serve as guideposts to ensure a prosperous and sustainable future for all members of our planet. Goal No. 7 is: Ensure access to clean, affordable, reliable, sustainable, and modern energy. Clean, affordable energy is the key to realizing the All Electric Society. The path to achieving this goal requires sustainable infrastructure design for all sectors that generate and consume energy. Achieving the goal of AES requires the comprehensive electrification, networking, and automation of all sectors of the economy while maximizing the potential in three key areas relating to energy. They are: • Renewable energy • Energy conservation • Energy recovery There are many initiatives that are being promoted by water industry groups, government agencies, and utilities that tie into this discussion. Many utilities are implementing principles of AES, even if they don’t realize they are. AES and water As previously noted, the U.N. SDGs identified clean, affordable electricity as a key to sustainability. So is Goal No. 6: Ensure availability and sustainable management of water and sanitation. It is important that we develop techniques to conserve and provide this resource to all. Reduced dependency on carbon energy, increased efficiency, and energy recovery are all important facets of the AES/water conversation. A good example that links AES with water is the Fall 2021 vote by the Los Angeles City Council to implement LA100, a plan for the L.A. Department of Water and Power (LADWP) — the nation’s largest utility — to transition to 100 percent clean energy by 2035. The plan is to replace L.A.’s natural gas electricity generation with wind, solar, and battery storage. It is an aggressive plan, but it is a clear indication of where the industry is heading. However, AES is more than replacing carbon-based energy with renewable energy. It also involves energy conservation through energy efficiency, an important component of the LA100 plan to cut demand. Per the Environmental Protection Agency (EPA), drinking water and wastewater plants are the largest energy consumers for many municipal governments, often accounting for 30 to 40 of total energy consumed by the municipality, while emitting over 45 million tons of greenhouse gases annually. Municipalities can reduce energy consumption by 15 to 30 percent and significantly reduce costs by incorporating energy- efficiency practices. However, to generate sufficient momentum for There are other examples of how the AES the energy revolution, solutions for AES must be as economical and cost-efficient as possible. Technical innovations and methods will play an important role in making AES a reality. A 2020 report by the World Economic Forum found that technology will play a critical role in achieving a majority of the SDGs. conversation is playing out in the water sector while encompassing the concept of the circular economy through resource and energy recovery. Wastewater treatment plants (WWTPs) are evolving into water resource recovery facilities (WRRFs) that produce clean water, nutrients, valuable bio-based materials, 20 UPDATE 6/22 The Phoenix Contact innovation magazine