Simplify industrial GSM/GPRS cellular modem service
MIDDLETOWN, Pa. - As an industrial GSM/GPRS modem provider, Phoenix Contact recognizes that finding the correct service plan can be one of the biggest challenges in deploying GSM/GPRS modems on the AT&T network. To solve this issue, Phoenix Contact has partnered with Stanza Systems, a GSM/GPRS service provider, to create a Diversenet, modem package that is easy to set up and deploy.
All Phoenix Contact GSM/GPRS modems ship with a pre-installed SIM card that can be activated by visiting the Diversenet portal. Using the Diversenet modem package, there is no need to contact AT&T, find the correct representative for the service needed, and sign a long-term service agreement.
The Diversenet portal provides an easy interface to activate the Phoenix Contact GSM/GPRS modem. It offers a variety of services, data and SMS options. There are no commitments or contracts to sign. After activating the GSM/GPRS modem via the portal network, communications are typically available in less than 10 minutes.
Diversenet allows three types of data communication: Dynamic IP, Virtual Static IP, and VPN secure networks. Each data option provides a unique way of accessing information from the devices attached to the GSM/GPRS modem. This connectivity spans from the traditional dynamic IP addressing services to private network access creating a static IP address, allowing the remote GSM/GPRS modem to be accessible at all times.
Phoenix Contact is a world leader in electrical connection, electronic interface and industrial automation technologies. A global company with annual sales exceeding 1 billion euro, Phoenix Contact GmbH & Co., Blomberg, Germany, operates 46 international subsidiaries, including Phoenix Contact USA in Middletown, Pa. Phoenix Contact's formal Integrated Management Systems meet International Standards Organization (ISO) quality, environmental and safety requirements (ISO 9001:2008,14001:2004 and 18001:2007).
Stanza Systems, Inc. provides data solutions and custom software development services that help companies benefit from the latest infrastructure monitoring technology. Stanza Systems has specialized expertise dealing with wireless and wired network engineering, real-time application integration, SCADA systems, network security, and service delivery management. Stanza is uniquely positioned to offer end-to-end M2M solutions for a wide range of information on demand needs including SCADA, meter reading, distribution system operations, asset management and general data gathering.
For more information on the GSM/GPRS modem or any other Phoenix Contact products, visit www.phoenixcontact.com, or call the Phoenix Contact Technical Service Department at 1-800-322-3225, e-mail info@phoenixcon.com.
###

Media Contact
Molly McGowan
717-944-1300 x3721
Email: mmcgowan@phoenixcon.com