Power supply units - Top of every class in technology
The reliability of a power supply unit is the decisive factor for the availability of complex systems. Phoenix Contact has therefore perfected the power supply units for industrial use.
These are some of the outstanding features of the power supply units from Phoenix Contact:
- Worldwide application due to the wide-range input and international approval package
- High operating safety due to long mains buffering under full load and high MTBF (> 500,000 h)
- Parallel connection possible for increased performance and redundancy
- Simplified startup thanks to LED function monitoring.

STEP POWER
Now with double performance density and maximum energy efficiency.

MINI POWER with integrated UPS
It has extensive signaling and optimized battery management.

TRIO POWER with special voltages
This has opened up new areas of application with 12 and 48 V DC output voltages.

QUINT POWER

SFB technology
For the first time ever, even the standard power circuit breakers can now be tripped reliably and quickly using the SFB technology with six times the nominal current for 12 ms.
Faulty current paths are switched off selectively, the fault is located and important system parts remain in operation.

Exhibitions & Dates
Do you wish to experience our products live? You can find us at the following exhibitions. We look forward to meeting you.