The application

System versions (point-to-point, multipoint)

Transmission from a sender to the corresponding receiver is the standard application, but it as also possible to use it as a wireless signal multiplication system. Transmission from a transmitter to several receivers is realized by teaching additional receivers the hop sequence of the common transmitter. In this configuration, the information can be distributed by the transmitter to several receivers.


Accessories


The uinidirectional RAD-ISM-2400-SET-UD-ANT set is supplied complete with standard antennae. Should directional antennae, adapters, or extensions for the antennae cables be necessary, tested and approved components are available. Signal converters and power supply units are also available from the Phoenix Contact range, as is surge protection.



Further information and services related to this article