Surge protection for worldwide use - VALVETRAB compact

VALVETRAB compact, the worldwide narrowest surge protection arrester with certification for all types of networks
VALVETRAB compact makes space in the control cabinet, now even with UL rating. There are compact solutions for all common US-specific power supply systems. With a width of just 12 mm per channel, this Class 2 surge arrester is the slimmest in the world and still has excellent performance data. The surge arresters have passed the tests in acc. with the requirements of UL 1449 and are identified with the corresponding mark of conformity on the label on the side.

But it is not only the technical data that make this surge arrester the product of choice. VALVETRAB compact has rotating base elements and plugs. It therefore makes no difference, whether the feed lines come in from above, as, for example, in industrial installations, or from below as in building installation. VALVETRAB compact fits in anywhere, and the marking is always legible. Time-consuming work on the installation is a thing of the past. Just pull out the plug and insulation measurements, for example, are no problem. Another plus for the arrester is the fact that it can be tested with CHECKMASTER. It allows you to carry out the tests required by the standards easily and conveniently.
With VALVETRAB compact, you're on the safe side without wasting any space in the control cabinet.
Convenient to use thanks to the rotatable base elements and plugs