Surge protection in the distribution cabinet


If you wish to transmit your data along high-speed networks and protect them against surge voltages, then you will find it hard to ignore the new D-LAN-19" distribution cabinet solution from Phoenix Contact.

Availability, particularly in high-speed data networks with up to 100 Mbps (Class D or category 5e), plays a crucial role. And testing in an independent test laboratory shows that Phoenix Contact has taken this role seriously: We are the only supplier worldwide to have fulfilled the requirements for Class D / CAT 5e applications and received the necessary certification.

Following D-LAN-CAT.5e, D-LAN-19" is now yet another product that fulfills the requirements of transmission quality in accordance with category 5e.

Universal surge protection for a range of data systems



Structure and fields of application


  • D-LAN-19" protects all signal conductors equally.
    Since all conductors are equally protected, protection is guaranteed no matter what the conductor pair assignment is. Surge protection is therefore ensured at all times.
  • Protection and comfort in the distribution cabinet
    You can choose between four and 24 protected ports over one height unit. In contrast to solutions offered by other suppliers, where connecting cables to surge protection at a later date is a complex matter, the front cabling makes it child's play.
  • Data transmission systems supported
    Due to the structure of the protective circuit, D-LAN-19" is a true all-rounder when it comes to supporting data transmission systems. ETHERNET, Token-Ring, and CDDI (FDDI), as well as the transmission systems of the future that will be operated with eight signal conductors, are protected with just one product. Switching from one system to the other is therefore also not a problem.
Use in the distribution cabinet