VALVETRAB compact – Surge protection for everyone
VALVETRAB compact makes space in the control cabinet, now even for power supply systems with 120 V ... 130 V AC nominal voltage. With a width of just 12 mm per channel, this type 2 surge arrester is the slimmest in the world and still has excellent performance data. The rated surge arrester voltage for all VAL-CP-...-175 types is 175 V AC. The arrester achieves a protection level of < 800 V. This also applies to protective paths between N and PE. UL-rating is also fulfilled with this performance data.

But it is not only the technical data that make this surge arrester the product of choice. VALVETRAB compact has rotating base elements and plugs. It therefore makes no difference, whether the feed lines come in from above, as, for example, in industrial installations, or from below as in building installation. VALVETRAB compact fits in anywhere, and the marking is always legible. Time-consuming work on the installation is a thing of the past. Just pull out the plug and insulation measurements, for example, are no problem. Another plus for the arrester is the fact that it can be tested with CHECKMASTER. It allows you to carry out the tests required by the standards easily and conveniently.
With VALVETRAB compact, you're on the safe side without wasting any space in the control cabinet.