CM-PA-FLT/VAL-CP - CHECKMASTER test socket

What are the arguments for it?

  • State-of-the-art testing
  • The world's first tester for spark gaps
  • One test socket for all FLT-CP/VAL-CP plug versions


Pluggability pays off


The universally pluggable FLASHTRAB compact and VALVETRAB compact surge protection devices can now also be tested. It is thus possible to carry out the regular checks on lightning protection systems fast and conveniently as required in VDE V 0185-3. Just unplug the plug, test it, and plug it back in. CHECKMASTER takes care of the protocol!



One for all

The newly developed CM-PA-FLT/VAL-CP test adapter has such a versatile design, that both VAL-CP and FLT-CP connectors can be tested in combination with CHECKMASTER. This also applies to the total current spark gap FLT-CP-N/PE.


Professional testing


An absolute innovation is the testing of spark gaps. But even the testing of Class II VAL-CP... arresters holds something new in store. With the CHECKMASTER, it is now possible to carry out more than just a simple function check. The special test procedure makes it possible to detect and log arresters that are already damaged. These arresters can then be replaced, providing markedly more safety and system availability.

Testing for FLASHTRAB compact and VALVETRAB compact modules sets new standards and helps you in the choice of the right surge protection.

FLASHTRAB compact



Further information and services related to this article



PHOENIX CONTACT GmbH & Co. KG
Flachsmarktstr. 8
D-32825 Blomberg
Phone: +49 (0) 5235-3 00
Fax: +49 (0) 5235-34 12 00