CHECKMASTER – Arrester testing at the highest level

Testing surge arresters is recommended by the lighting protection directive of the VdS (Verband der Sachversicherer – Property Insurer Association) and in the German standard DIN V VDE V 0185 – Part 3. This test can be carried out easily, safely and reliably with the CHECKMASTER, the arrester test device for all plug-in surge arresters from Phoenix Contact.


The CHECKMASTER is an intelligent testing device. Intelligent, because the CHECKMASTER includes the objects of the test component in the arrester test. It has been proven in practice that in order to get exact information regarding the state of an arrester, a purely thermic or mechanical test of individual components is not sufficient. For this reason, CHECKMASTER checks the electrical parameters of the protective plug components.

Taking the tolerance limits into account, an assertion can be made regarding potential pre-damage to the surge arrester. On the display and in the log, such predamage is documented with the note: "Tolerance limit reached. Exchange recommended".

The CHECKMASTER gives you X-ray vision
The CHECKMASTER gives you X-ray vision



To provide a permanent record, CHECKMASTER has an RS-232/C, V-24 interface to which a PC or printer can be connected. The results of the individual arrester tests can thus be printed out and processed in a protocol with date, time and other identification.

The CHECKMASTER provides more functions than this one.

  • Simple test sequence: Selecting, scanning, testing, logging
  • Cost-effective thanks to "on-site testing"
  • Update via Internet, which saves on shipping costs for updating
  • Extendable through modular test cassettes


Summary


CHECKMASTER – The test device for all plug-in surge arresters from Phoenix Contact
CHECKMASTER – The test device for all plug-in surge arresters from Phoenix Contact
Extensive surge protection does not end with the use of the right products, but includes the standardized requirements for testing. System availability and the associated reliability of your plant is further increased with the CHECKMASTER.

Regular testing of your arresters saves you extra maintenance work and the associated costs. With surge protection from Phoenix Contact, you are safe no matter what – from consulting, through to products and on to support and maintenance and testing.




Further information and services related to this article



PHOENIX CONTACT GmbH & Co. KG
Flachsmarktstr. 8
D-32825 Blomberg
Phone: +49 (0) 5235-3 00
Fax: +49 (0) 5235-34 12 00