Solution Center HOUSING


Phoenix Contact provides DIN rail mountable electronic housings for PCBs from just a few square centimeters up to the Euro-card format.
To implement customer-specific housing variants, each housing of the comprehensive standard range can be modified. A highly motivated team in the "Solution Center HOUSING" is armed for all challenges. Housing modification, printing and color variants are all reliably put into practice.




Special cutouts can be made using mechanical processes such as milling or punching or adding customer-specific tool inserts. Labeling and printing also poses no problem. Tampon or laser printing guarantee high-quality print.



To ensure reliable exchange of information, COMBICON Select allows you to download drawings in various formats and make use of them for processing and printing templates. Just return them to us as a file by e-mail or as a printout. We will start work on them immediately.

We have a comprehensive store of different granulates for the manufacture of customer-specific special colors.



In addition to modifying standard housings, it is also possible to develop individual special housings. As soon as we have the requirements and an agreement has been reached on an economically viable batch size, Phoenix Contact constructs and manufactures tailor-made electronic housings. The sooner the cooperation between housing manufacturer and electronic developer starts, the easier it is to develop a functional and innovative housing.



The "Solution Center HOUSING" guarantees fast implementation of all customer-specific requirements. The integrated connection method guarantees a professional overall solution and turns your electronics into a perfect product for the market.


Further information and services related to this article



PHOENIX CONTACT GmbH & Co. KG
Flachsmarktstr. 8
D-32825 Blomberg
Phone: +49 (0) 5235-3 00
Fax: +49 (0) 5235-34 12 00