The PTDA terminal block range with double connection is now even more flexible
This series has been supplemented with two pitch spacers in pitches of 3.5 mm and 5.0 mm.
If desired, distance pieces with an integrated window on the front side of the terminal block are also available.
If the user places an LED below the pitch spacer, the light shines through the window. Different operating states of the circuit can thus be visualized.
- Further information on spring-cage compact terminal blocks
- PCB connection technology for building automation