Protection for HBUS connectors for the BC housing

The  16-pos. HBUS DIN rail bus connectors of the BC installation housing can transmit parallel as well as serial data.


This bus connector is initially snapped on to the DIN rail.The BC housing is then placed on this bus connector, and is then in contact.The unneeded contact rows can be sealed with the new cover flaps.

The article set consists of three covers, which protect the HBUS connector with a perfect fit.It is easily mounted simply by snapping it on. It is dismantled by hand or with a screwdriver.

Protection for HBUS connectors for the BC housing
Protection for HBUS connectors for the BC housing



Further information and services related to this article



PHOENIX CONTACT GmbH & Co. KG
Flachsmarktstr. 8
D-32825 Blomberg
Phone: +49 (0) 5235-3 00
Fax: +49 (0) 5235-34 12 00