A new record – 125 A plugged onto the PCB!

PC 35, the new printed circuit board connector, has a current carrying capacity of up to 125 A. This makes it the only printed circuit board connector in the market capable of transferring such a high current.


Thanks to the low insertion and withdrawal forces, device connections can be very easily established even in the high performance class. With a screw terminal block, conductors up to 35 mm² can be safely connected using the tension sleeve principle.

The 2 to 6-position connectors are always equipped with a screw flange that safely connects the connector to the base strip. It can also be used simultaneously as a panel feed-through on the base strip side, thus providing additional support in the device.




Professional shield connection

In the case of a 15 mm pitch, the PC 35 connectors always have the unrestricted 600 V UL approval (UL1059) and 1000 V as per IEC. Connectors and base strips are also available as 4-position variants with a professional shield connection.

You can test the PC 35 and all new products live at electronica 2008 in Munich.