PCB terminal block with snap-on mechanism in the housing
Todays building automation requirements demand modern devices to be compact and powerful. Miniaturization often leads to restricted spaces, thus making conductor connection difficult.
The new terminal block range PT 1,5…CLIP is designed for devices with a clam-shell housing. The connection is conveniently established on the header of the device. After the connection has been established the electronic system is placed on the header and makes contact with the terminal block via a pin strip.
The device can be mounted beforehand. The electronic system is not subjected to any harm and can be replaced in the case of an error without the need for wiring.