Flexible connection method with spring-cage technology

The new series with PCB terminal blocks and connectors with the PTDA spring-cage double connection from Phoenix Contact now provides two connections per electric potential, which simplifies the looping through of conductors. The terminal points are arranged at an angle of 45° to the PCB.


The round and symmetrical PCB terminal blocks are available as a pluggable or fixed, solderable version with a 3.5 mm to 5.0 mm pitch. The disk design and uniform shape allow for individual blocks in mixed pitches, which can also be color-coded. This makes is easier for the user to safely install the devices to be connected without errors.



With their connection capacities of of 2 x 2.5 mm² / 2 x 1.5 mm² (solid / stranded), the PCB terminal block is fitted to the usual conductor cross-sections in building installation and thus provides a large terminal capacity with direct plug-in technology. With the convenient release button, the conductors can be quickly released again, if needed.

Thanks to the symmetric design, the PCBs can be accommodated in the housing horizontally or vertically. The outer appearance of the terminal blocks remain the same.