New sensor/actuator boxes with M12 rapid interlock system for medium mechanical stresses
The new sensor/actuator box product range was presented at the 2011 Hanover fair.
The distributors are optimized for medium mechanical stresses, such as those in packaging equipment or machine construction.
The robust housing is fully sealed and has the proven SPEEDCON rapid interlock system, which is integrated into the plastic housing.
Highly diverse range
The range includes sensor/actuator boxes with firmly connected trunk line, spring-cage connection, and plug-in screw connection.
In addition, you can separately order the header and connector hoods for the screw connection in order to create separate storage.
You will get all versions with four, six or eight slots that are each single- or double-wired.