Sensor/actuator box replaces M12 panel feed-throughs

The sensor/actuator box with rear and pluggable spring-cage connection is directly mounted on the control cabinet panel. An appropriate mounting cutout is the only preparation needed. The grommet at the rear side of the box is used for sealing.


In the control cabinet, the litz wires can be directly connected via the push-in spring-cage connection and provide easily disconnectable connections thanks to the pluggable design.

The customary features of the SPEEDCON sensor/actuator box are available outside the control cabinet. It can be connected with sensors or actuators using standardized M12 connectors and sensor/actuator cables.

M12 sensor/actuator box with rear, pluggable spring-cage connection
M12 sensor/actuator box with rear, pluggable spring-cage connection



The benefits at a glance

  • A mounting cutout for eight M12 plug-in connections
  • Pluggable connection in the control cabinet
  • Marking the slots
  • Visual status display
  • SPEEDCON fast connection technology


Further information and services related to this article



PHOENIX CONTACT GmbH & Co. KG
Flachsmarktstr. 8
D-32825 Blomberg
Phone: +49 (0) 5235-3 00
Fax: +49 (0) 5235-34 12 00